Files | |
file | lib/include/est.h [code] |
Contains the public interface to the estimator (EST) module routines simplify est.h for software library. | |
file | lib/include/est_Flux_states.h [code] |
file | lib/include/est_Ls_states.h [code] |
file | lib/include/est_Rr_states.h [code] |
file | lib/include/est_Rs_states.h [code] |
file | lib/include/est_states.h [code] |
file | lib/include/est_Traj_states.h [code] |
file | lib/include/motor.h [code] |
file | lib/include/userParams.h [code] |
Contains the public interface for the HAL and EST modules (floating point) userParams.h for FAST software library. | |