Go to the documentation of this file.
37 #ifndef EST_TRAJ_STATES_H
38 #define EST_TRAJ_STATES_H
115 #endif // end of EST_TRAJ_STATES_H definition
the number of trajectory generator error codes
Definition: lib/include/est_Traj_states.h:74
reserved to force 32 bit data
Definition: lib/include/est_Traj_states.h:98
EST_Traj_ErrorCode_e
Enumeration for the trajectory generator error codes.
Definition: lib/include/est_Traj_states.h:70
the trajectory generator parameter estimation state
Definition: lib/include/est_Traj_states.h:95
no error error code
Definition: lib/include/est_Traj_states.h:72
EST_Traj_State_e
Enumeration for the trajectory generator states.
Definition: lib/include/est_Traj_states.h:91
the trajectory generator online state
Definition: lib/include/est_Traj_states.h:96
the trajectory generator error state
Definition: lib/include/est_Traj_states.h:93
the trajectory generator idle state
Definition: lib/include/est_Traj_states.h:94
Id clip error code.
Definition: lib/include/est_Traj_states.h:73
the number of trajectory generator states
Definition: lib/include/est_Traj_states.h:97
Copyright 2023, Texas Instruments Incorporated