![]() |
![]() |
Defines the DRV8353 object. More...
#include <drv8353s.h>
Data Fields | |
uint32_t | spiHandle |
handle for the serial peripheral interface More... | |
uint32_t | gpioNumber_CS |
GPIO connected to the DRV8353 CS pin. More... | |
uint32_t | gpioNumber_EN |
GPIO connected to the DRV8353 enable pin. More... | |
bool | rxTimeOut |
timeout flag for the RX FIFO More... | |
bool | enableTimeOut |
timeout flag for DRV8353 enable More... | |
Defines the DRV8353 object.
uint32_t _DRV8353_Obj_::spiHandle |
handle for the serial peripheral interface
uint32_t _DRV8353_Obj_::gpioNumber_CS |
GPIO connected to the DRV8353 CS pin.
uint32_t _DRV8353_Obj_::gpioNumber_EN |
GPIO connected to the DRV8353 enable pin.
bool _DRV8353_Obj_::rxTimeOut |
timeout flag for the RX FIFO
Referenced by DRV8353_resetRxTimeout().
bool _DRV8353_Obj_::enableTimeOut |
timeout flag for DRV8353 enable
Referenced by DRV8353_resetEnableTimeout().