![]() |
![]() |
Object for the DRV8353 registers and commands. More...
#include <drv8353s.h>
Data Fields | |
union DRV8353_STAT00_REG | statReg00 |
union DRV8353_STAT01_REG | statReg01 |
union DRV8353_CTRL02_REG | ctrlReg02 |
union DRV8353_CTRL03_REG | ctrlReg03 |
union DRV8353_CTRL04_REG | ctrlReg04 |
union DRV8353_CTRL05_REG | ctrlReg05 |
union DRV8353_CTRL06_REG | ctrlReg06 |
union DRV8353_CTRL07_REG | ctrlReg07 |
bool | writeCmd |
bool | readCmd |
uint16_t | manWriteAddr |
uint16_t | manReadAddr |
uint16_t | manWriteData |
uint16_t | manReadData |
bool | manWriteCmd |
bool | manReadCmd |
Object for the DRV8353 registers and commands.
union DRV8353_STAT00_REG _DRV8353_VARS_t_::statReg00 |
union DRV8353_STAT01_REG _DRV8353_VARS_t_::statReg01 |
union DRV8353_CTRL02_REG _DRV8353_VARS_t_::ctrlReg02 |
union DRV8353_CTRL03_REG _DRV8353_VARS_t_::ctrlReg03 |
union DRV8353_CTRL04_REG _DRV8353_VARS_t_::ctrlReg04 |
union DRV8353_CTRL05_REG _DRV8353_VARS_t_::ctrlReg05 |
union DRV8353_CTRL06_REG _DRV8353_VARS_t_::ctrlReg06 |
union DRV8353_CTRL07_REG _DRV8353_VARS_t_::ctrlReg07 |
bool _DRV8353_VARS_t_::writeCmd |
bool _DRV8353_VARS_t_::readCmd |
uint16_t _DRV8353_VARS_t_::manWriteAddr |
uint16_t _DRV8353_VARS_t_::manReadAddr |
uint16_t _DRV8353_VARS_t_::manWriteData |
uint16_t _DRV8353_VARS_t_::manReadData |
bool _DRV8353_VARS_t_::manWriteCmd |
bool _DRV8353_VARS_t_::manReadCmd |