Object for the DRV8353 CTRL02 register. More...
#include <drv8353s.h>
Data Fields | |
bool | CLR_FLT:1 |
bool | BRAKE:1 |
bool | COAST:1 |
bool | PWM1_DIR:1 |
bool | PWM1_COM:1 |
DRV8353_CTRL02_PWMMode_e | PWM_MODE:2 |
bool | OTW_REP:1 |
bool | DIS_GDF:1 |
bool | DIS_GPUV:1 |
bool | OCP_ACT:1 |
uint16_t | rsvd2:5 |
Object for the DRV8353 CTRL02 register.
bool DRV8353_CTRL02_BITS::CLR_FLT |
bool DRV8353_CTRL02_BITS::BRAKE |
bool DRV8353_CTRL02_BITS::COAST |
bool DRV8353_CTRL02_BITS::PWM1_DIR |
bool DRV8353_CTRL02_BITS::PWM1_COM |
DRV8353_CTRL02_PWMMode_e DRV8353_CTRL02_BITS::PWM_MODE |
bool DRV8353_CTRL02_BITS::OTW_REP |
bool DRV8353_CTRL02_BITS::DIS_GDF |
bool DRV8353_CTRL02_BITS::DIS_GPUV |
bool DRV8353_CTRL02_BITS::OCP_ACT |
uint16_t DRV8353_CTRL02_BITS::rsvd2 |