![]() |
![]() |
Object for the DRV8353 CTRL04 register. More...
#include <drv8353s.h>
Data Fields | |
DRV8353_CTRL04_PeakSinkCurLS_e | IDRIVEN_LS:4 |
DRV8353_CTRL04_PeakSourCurLS_e | IDRIVEP_LS:4 |
DRV8353_CTRL04_PeakTime_e | TDRIVE:2 |
bool | CBC:1 |
uint16_t | rsvd:5 |
Object for the DRV8353 CTRL04 register.
DRV8353_CTRL04_PeakSinkCurLS_e DRV8353_CTRL04_BITS::IDRIVEN_LS |
DRV8353_CTRL04_PeakSourCurLS_e DRV8353_CTRL04_BITS::IDRIVEP_LS |
DRV8353_CTRL04_PeakTime_e DRV8353_CTRL04_BITS::TDRIVE |
bool DRV8353_CTRL04_BITS::CBC |
uint16_t DRV8353_CTRL04_BITS::rsvd |