Object for the DRV8353 CTRL06 register. More...
#include <drv8353s.h>
Data Fields | |
bool | CAL_MODE:1 |
uint16_t | rsvd1:10 |
uint16_t | rsvd2:5 |
Object for the DRV8353 CTRL06 register.
bool DRV8353_CTRL07_BITS::CAL_MODE |
uint16_t DRV8353_CTRL07_BITS::rsvd1 |
uint16_t DRV8353_CTRL07_BITS::rsvd2 |