![]() |
![]() |
Go to the source code of this file.
Data Structures | |
struct | _PHVOLC_Obj_ |
Defines the PHVOLC controller object. More... | |
Macros | |
#define | VC_ONE_THIRD 0.33333333333333f |
#define | VC_TWO_THIRD 0.66666666666667f |
#define | VC_INV_SQRT3 0.57735026918963f |
Typedefs | |
typedef struct _PHVOLC_Obj_ | PHVOLC_Obj |
Defines the PHVOLC controller object. More... | |
typedef struct _PHVOLC_Obj_ * | PHVOLC_Handle |
Defines the PHVOLC handle. More... | |
Functions | |
static void | PHVOLC_run (PHVOLC_Handle handle, float32_t Vdcbus, MATH_Vec3 *pVabc_pu, MATH_Vec2 *pVab_V) |