Go to the documentation of this file.
67 #define VC_ONE_THIRD 0.33333333333333f
68 #define VC_TWO_THIRD 0.66666666666667f
69 #define VC_INV_SQRT3 0.57735026918963f
123 #endif // end of VOLT_CAL_H defines
Defines a two element vector.
Definition: math.h:218
float32_t VphaseB
Definition: volt_calc.h:46
float float32_t
Definition: sfra_f32.h:42
float32_t VphaseC
Definition: volt_calc.h:47
#define VC_INV_SQRT3
Definition: volt_calc.h:69
uint16_t flagOutOfPhase
Definition: volt_calc.h:50
struct _PHVOLC_Obj_ PHVOLC_Obj
Defines the PHVOLC controller object.
Defines the PHVOLC controller object.
Definition: volt_calc.h:43
float32_t value[3]
Definition: math.h:232
float32_t Valpha
Definition: volt_calc.h:48
float32_t Vbeta
Definition: volt_calc.h:49
static void PHVOLC_run(PHVOLC_Handle handle, float32_t Vdcbus, MATH_Vec3 *pVabc_pu, MATH_Vec2 *pVab_V)
Definition: volt_calc.h:74
float32_t VphaseA
Definition: volt_calc.h:45
#define VC_ONE_THIRD
Definition: volt_calc.h:67
struct _PHVOLC_Obj_ * PHVOLC_Handle
Defines the PHVOLC handle.
Definition: volt_calc.h:58
Defines a three element vector.
Definition: math.h:230
Copyright 2023, Texas Instruments Incorporated