TI BLE-Stack for Bluetooth 4.2 API Documentation
3.02.03.00
|
Parameter Structure to add new Characteristic Description Response SNP_ADD_CHAR_DESC_DECL_RSP. More...
Data Fields | |
uint16_t | handles [6] |
Maximum handles returned is 6. One for each possible attribute added. Header will determine the number of actual handles returned. | |
uint8_t | header |
uint8_t | status |
1 Byte Command Status list of status generated by the SNP. | |
Parameter Structure to add new Characteristic Description Response SNP_ADD_CHAR_DESC_DECL_RSP.
snpAddCharDescDeclRsp_t::handles will be populated with attributes added based on the header, starting from LSB to MSB.
This packet structure is not used to create a NPI frame