TI BLE-Stack for Bluetooth 4.2 API Documentation  3.02.03.00
snp.h
Go to the documentation of this file.
1 /******************************************************************************
2 
3  @file snp.h
4 
5  @brief main header file for the serial network processor
6 
7  Group: WCS, BTS
8  $Target Device: DEVICES $
9 
10  ******************************************************************************
11  $License: BSD3 2015 $
12  ******************************************************************************
13  $Release Name: PACKAGE NAME $
14  $Release Date: PACKAGE RELEASE DATE $
15  *****************************************************************************/
16 
25 #ifndef SNP_H
26 #define SNP_H
27 
28 #ifdef __cplusplus
29 extern "C"
30 {
31 #endif
32 
33 /*********************************************************************
34  * INCLUDES
35  */
36 
37 #include "hal_types.h"
38 
39 /*********************************************************************
40 * EXTERNAL VARIABLES
41 */
42 
48 /*********************************************************************
49  * CONSTANTS
50  */
51 
53 #define SNP_IMAGE_START 0x00000000
54 
56 
59 #define SNP_NPI_ASYNC_CMD_TYPE (RPC_SYS_BLE_SNP+(NPI_MSG_TYPE_ASYNC<<5))
61 #define SNP_NPI_SYNC_REQ_TYPE (RPC_SYS_BLE_SNP+(NPI_MSG_TYPE_SYNCREQ<<5))
63 #define SNP_NPI_SYNC_RSP_TYPE (RPC_SYS_BLE_SNP+(NPI_MSG_TYPE_SYNCRSP<<5))
65 
69 // Fixed size, must not exceed 2 bits!
71 // the upper two bits of NPI frame cmd1 field is reserved for subgroup value.
73  SNP_DEVICE_GRP = 0,
74  SNP_GAP_GRP,
75  SNP_GATT_GRP,
76  SNP_RFU_GRP
77 };
78 
83 #define SNP_MASK_EVT_REQ 0x02
84 #define SNP_GET_REVISION_REQ 0x03
85 #define SNP_HCI_CMD_REQ 0x04
86 #define SNP_GET_STATUS_REQ 0x06
87 #define SNP_GET_RAND_REQ 0x07
88 #define SNP_TEST_REQ 0x10
89 
95 #define SNP_POWER_UP_IND 0x01
96 #define SNP_MASK_EVENT_RSP 0x02
97 #define SNP_GET_REVISION_RSP 0x03
98 #define SNP_HCI_CMD_RSP 0x04
99 #define SNP_EVENT_IND 0x05
100 #define SNP_GET_STATUS_RSP 0x06
101 #define SNP_SYNC_ERROR_CMD_IND 0x07
102 #define SNP_GET_RAND_RSP 0x08
103 #define SNP_TEST_RSP 0x10
104 
110 #define SNP_INIT_DEVICE_REQ 0x41
111 #define SNP_START_ADV_REQ 0x42
112 #define SNP_SET_ADV_DATA_REQ 0x43
113 #define SNP_STOP_ADV_REQ 0x44
114 #define SNP_UPDATE_CONN_PARAM_REQ 0x45
115 #define SNP_TERMINATE_CONN_REQ 0x46
116 #define SNP_SET_GAP_PARAM_REQ 0x48
117 #define SNP_GET_GAP_PARAM_REQ 0x49
118 #define SNP_SET_SECURITY_PARAM_REQ 0x4A
119 #define SNP_SEND_SECURITY_REQUEST_REQ 0x4B
120 #define SNP_SET_AUTHENTICATION_DATA_REQ 0x4C
121 #define SNP_SET_WHITE_LIST_POLICY_REQ 0x4D
122 
128 #define SNP_INIT_DEVICE_CNF 0x41
129 #define SNP_SET_ADV_DATA_CNF 0x43
130 #define SNP_UPDATE_CONN_PARAM_CNF 0x45
131 #define SNP_SET_GAP_PARAM_RSP 0x48
132 #define SNP_GET_GAP_PARAM_RSP 0x49
133 #define SNP_SET_SECURITY_PARAM_RSP 0x4A
134 #define SNP_SEND_AUTHENTICATION_DATA_RSP 0x4C
135 #define SNP_SET_WHITE_LIST_POLICY_RSP 0x4D
136 
142 #define SNP_ADD_SERVICE_REQ 0x81
143 #define SNP_ADD_CHAR_VAL_DECL_REQ 0x82
144 #define SNP_ADD_CHAR_DESC_DECL_REQ 0x83
145 #define SNP_REGISTER_SERVICE_REQ 0x84
146 #define SNP_GET_ATTR_VALUE_REQ 0x85
147 #define SNP_SET_ATTR_VALUE_REQ 0x86
148 #define SNP_CHAR_READ_CNF 0x87
149 #define SNP_CHAR_WRITE_CNF 0x88
150 #define SNP_SEND_NOTIF_IND_REQ 0x89
151 #define SNP_CCCD_UPDATED_CNF 0x8B
152 #define SNP_SET_GATT_PARAM_REQ 0x8C
153 #define SNP_GET_GATT_PARAM_REQ 0x8D
154 #define SNP_REG_PREDEF_SRV_REQ 0x8E
155 
161 #define SNP_ADD_SERVICE_RSP 0x81
162 #define SNP_ADD_CHAR_VAL_DECL_RSP 0x82
163 #define SNP_ADD_CHAR_DESC_DECL_RSP 0x83
164 #define SNP_REGISTER_SERVICE_RSP 0x84
165 #define SNP_GET_ATTR_VALUE_RSP 0x85
166 #define SNP_SET_ATTR_VALUE_RSP 0x86
167 #define SNP_CHAR_READ_IND 0x87
168 #define SNP_CHAR_WRITE_IND 0x88
169 #define SNP_SEND_NOTIF_IND_CNF 0x89
170 #define SNP_CCCD_UPDATED_IND 0x8B
171 #define SNP_SET_GATT_PARAM_RSP 0x8C
172 #define SNP_GET_GATT_PARAM_RSP 0x8D
173 #define SNP_REG_PREDEF_SRV_RSP 0x8E
174 
179 #define SNP_SUCCESS 0x00
180 #define SNP_FAILURE 0x83
181 #define SNP_INVALID_PARAMS 0x84
182 #define SNP_CMD_ALREADY_IN_PROGRESS 0x85
183 #define SNP_CMD_REJECTED 0x86
184 #define SNP_OUT_OF_RESOURCES 0x87
185 #define SNP_UNKNOWN_ATTRIBUTE 0x88
186 #define SNP_UNKNOWN_SERVICE 0x89
187 #define SNP_ALREADY_ADVERTISING 0x8A
188 #define SNP_NOT_ADVERTISING 0x8B
189 #define SNP_HCI_RSP_COLLISION_RSP 0x8C
190 #define SNP_HCI_CMD_UNKNOWN 0x8D
191 #define SNP_GATT_COLLISION 0x8E
192 #define SNP_NOTIF_IND_NOT_ENABLE_BY_CLIENT 0x8F
193 #define SNP_NOTIF_IND_NOT_ALLOWED 0x90
194 #define SNP_NOTIF_IND_NO_CCCD_ATTRIBUTE 0x91
195 #define SNP_NOT_CONNECTED 0x92
196 #define SNP_FAILURE_NO_ATT_RSP 0x93
197 
209 #define SNP_BLE_NO_RESOURCES bleNoResources
210 #define SNP_BLE_GAP_BOND_REJECTED bleGAPBondRejected
211 #define SNP_BLE_MEM_ALLOC_ERROR bleMemAllocError
212 #define SNP_BLE_TIMEOUT bleTimeout
213 #define SNP_INVALIDPARAMETER INVALIDPARAMETER
214 
215 
222 #define SNP_LL_ENC_KEY_REQ_REJECTED LL_ENC_KEY_REQ_REJECTED
223 #define SNP_LL_ENC_KEY_REQ_UNSUPPORTED_FEATURE LL_ENC_KEY_REQ_UNSUPPORTED_FEATURE
224 #define SNP_LL_CTRL_PKT_TIMEOUT_TERM LL_CTRL_PKT_TIMEOUT_TERM
225 #define SNP_LL_STATUS_ERROR_BAD_PARAMETER LL_STATUS_ERROR_BAD_PARAMETER
226 #define SNP_LL_STATUS_ERROR_COMMAND_DISALLOWED LL_STATUS_ERROR_COMMAND_DISALLOWED
227 #define SNP_LL_STATUS_ERROR_FEATURE_NOT_SUPPORTED LL_STATUS_ERROR_FEATURE_NOT_SUPPORTED
228 #define SNP_LL_STATUS_ERROR_CTRL_PROC_ALREADY_ACTIVE LL_STATUS_ERROR_CTRL_PROC_ALREADY_ACTIVE
229 #define SNP_LL_STATUS_ERROR_INACTIVE_CONNECTION LL_STATUS_ERROR_INACTIVE_CONNECTION
230 
231 
238 #define SNP_SMP_PAIRING_FAILED_UNSPECIFIED SMP_PAIRING_FAILED_UNSPECIFIED
239 #define SNP_SMP_PAIRING_FAILED_NUM_COMPARISON_FAILED SMP_PAIRING_FAILED_NUM_COMPARISON_FAILED
240 #define SNP_SMP_PAIRING_FAILED_NOT_SUPPORTED SMP_PAIRING_FAILED_NOT_SUPPORTED
241 #define SNP_SMP_PAIRING_FAILED_PASSKEY_ENTRY_FAILED SMP_PAIRING_FAILED_PASSKEY_ENTRY_FAILED
242 #define SNP_SMP_PAIRING_FAILED_AUTH_REQ SMP_PAIRING_FAILED_AUTH_REQ
243 #define SNP_SMP_PAIRING_FAILED_ENC_KEY_SIZE SMP_PAIRING_FAILED_ENC_KEY_SIZE
244 #define SNP_SMP_PAIRING_FAILED_CMD_NOT_SUPPORTED SMP_PAIRING_FAILED_CMD_NOT_SUPPORTED
245 #define SNP_SMP_PAIRING_FAILED_OOB_NOT_AVAIL SMP_PAIRING_FAILED_OOB_NOT_AVAIL
246 #define SNP_SMP_PAIRING_FAILED_CONFIRM_VALUE SMP_PAIRING_FAILED_CONFIRM_VALUE
247 #define SNP_SMP_PAIRING_FAILED_DHKEY_CHECK_FAILED SMP_PAIRING_FAILED_DHKEY_CHECK_FAILED
248 
249 
253 #define SNP_CONN_EST_EVT 0x0001
254 #define SNP_CONN_TERM_EVT 0x0002
255 #define SNP_CONN_PARAM_UPDATED_EVT 0x0004
256 #define SNP_ADV_STARTED_EVT 0x0008
257 #define SNP_ADV_ENDED_EVT 0x0010
258 #define SNP_ATT_MTU_EVT 0x0020
259 #define SNP_SECURITY_EVT 0x0040
260 #define SNP_AUTHENTICATION_EVT 0x0080
261 #define SNP_ERROR_EVT 0x8000
262 
265 #define SNP_DEV_ALL_EVENT_MASK (SNP_CONN_EST_EVT | SNP_CONN_TERM_EVT | \
267 SNP_CONN_PARAM_UPDATED_EVT | SNP_ADV_STARTED_EVT | SNP_ADV_ENDED_EVT | \
268  SNP_ATT_MTU_EVT | SNP_ERROR_EVT)
269 
270 /* HCI Opcodes */
274 #define SNP_HCI_OPCODE_EXT_SET_TX_POWER 0xFC01
275 #define SNP_HCI_OPCODE_EXT_MODEM_TEST_TX 0xFC08
276 #define SNP_HCI_OPCODE_EXT_MODEM_HOP_TEST_TX 0xFC09
277 #define SNP_HCI_OPCODE_EXT_MODEM_TEST_RX 0xFC0A
278 #define SNP_HCI_OPCODE_EXT_END_MODEM_TEST 0xFC0B
279 #define SNP_HCI_OPCODE_EXT_SET_BDADDR 0xFC0C
280 #define SNP_HCI_OPCODE_EXT_SET_SCA 0xFC0D
281 #define SNP_HCI_OPCODE_EXT_ENABLE_PTM 0xFC0E
282 #define SNP_HCI_OPCODE_EXT_SET_MAX_DTM_TX_POWER 0xFC11
283 #define SNP_HCI_OPCODE_EXT_RESET_SYSTEM 0xFC1D
284 #define SNP_HCI_OPCODE_READ_BDADDR 0x1009
285 #define SNP_HCI_OPCODE_READ_RSSI 0x1405
286 #define SNP_HCI_OPCODE_LE_RECEIVER_TEST 0x201D
287 #define SNP_HCI_OPCODE_LE_TRANSMITTER_TEST 0x201E
288 #define SNP_HCI_OPCODE_LE_TEST_END 0x201F
289 #define SNP_HCI_OPCODE_EXT_PER 0xFC14
290 #define SNP_HCI_OPCODE_EXT_DECRYPT 0xFC05
291 #define SNP_HCI_OPCODE_LE_ENCRYPT 0x2017
292 #define SNP_HCI_OPCODE_EXT_OVERRIDE_SL 0xFC1A
293 #define SNP_HCI_OPCODE_EXT_SET_FAST_TX_RESP_TIME 0xFC07
294 #define SNP_HCI_OPCODE_EXT_ONE_PKT_PER_EVT 0xFC02
295 #define SNP_HCI_OPCODE_EXT_GET_CONNECTION_INFO 0xFC20
296 
300 #define SNP_HCI_OPCODE_SIZE 0x02
302 
303 
304 /* Advertising */
308 #define SNP_ADV_TYPE_CONN 0x00
309 #define SNP_ADV_TYPE_SCANABLE 0x02
310 #define SNP_ADV_TYPE_NONCONN 0x03
311 
318 #define SNP_FILTER_POLICY_ALL 0x00
319 #define SNP_FILTER_POLICY_WHITE 0x03
320 
327 #define SNP_ADV_STOP_ON_CONN 0x00
329 #define SNP_ADV_RESTART_ON_CONN_EST 0x01
332 #define SNP_ADV_RESTART_ON_CONN_TERM 0x02
335 
342 #define SNP_SCANRSP_DATA 0x00 // Scan response data
344 #define SNP_NONCONN_ADV_DATA 0x01 // Non-connectable advertising data.
346 #define SNP_CONN_ADV_DATA 0x02 // Connectable advertising data.
348 
352 #define SNP_MAX_ADVDATA_LENGTH 31
354 
356 
359 #define SNP_CT_SUPERVISOR_TO 0x08
360 #define SNP_CT_PEER_REQ 0x13
361 #define SNP_CT_HOST_REQ 0x16
362 #define SNP_CT_CTRL_PKT_TO 0x22
363 #define SNP_CT_CTRL_PKT_INST_PASS 0x28
364 #define SNP_CT_LSTO_VIOLATION 0x3B
365 #define SNP_CT_MIC_FAILURE 0x3D
366 
370 /* Connection Parameters and Updates */
371 #define SNP_CONN_INT_MIN 0x0006
373 #define SNP_CONN_INT_MAX 0x0C80
374 
375 #define SNP_CONN_SL_MIN 0x0000
377 #define SNP_CONN_SL_MAX 0x01F3
378 
379 #define SNP_CONN_SUPERVISOR_TIMEOUT_MIN 0x000A
381 #define SNP_CONN_SUPERVISOR_TIMEOUT_MAX 0x0C80
382 
383 
386 #define SNP_PRIMARY_SERVICE 1
388 #define SNP_SECONDARY_SERVICE 2
390 
392 #define SNP_CHAR_MANAGED_BY_AP 0x00
393 #define SNP_CHAR_MANAGED_BY_NP 0x01
394 
395 
398 #define SNP_16BIT_UUID_SIZE 2
399 #define SNP_128BIT_UUID_SIZE 16
400 
405 #define SNP_GATT_PERMIT_READ 0x01
408 #define SNP_GATT_PERMIT_WRITE 0x02
410 #define SNP_GATT_PERMIT_AUTHEN_READ 0x04
412 #define SNP_GATT_PERMIT_AUTHEN_WRITE 0x08
414 #define SNP_GATT_PERMIT_ENCRYPT_READ 0x40
416 #define SNP_GATT_PERMIT_ENCRYPT_WRITE 0x80
418 
421 #define SNP_GATT_PERM_RFU_MASK (SNP_GATT_PERMIT_READ | \
423  SNP_GATT_PERMIT_WRITE | \
424  SNP_GATT_PERMIT_AUTHEN_READ | \
425  SNP_GATT_PERMIT_AUTHEN_WRITE | \
426  SNP_GATT_PERMIT_ENCRYPT_READ | \
427  SNP_GATT_PERMIT_ENCRYPT_WRITE)
428 
432 #define SNP_GATT_PROP_READ 0x0002
433 #define SNP_GATT_PROP_WRITE_NORSP 0x0004
434 #define SNP_GATT_PROP_WRITE 0x0008
435 #define SNP_GATT_PROP_NOTIFICATION 0x0010
436 #define SNP_GATT_PROP_INDICATION 0x0020
437 
439 #define SNP_GATT_CHAR_MAX_LENGTH 512
441 
445 #define SNP_SEND_NOTIFICATION 0x01
447 #define SNP_SEND_INDICATION 0x02
449 
455 #define SNP_GGS_SERV_ID 0x01
456 #define SNP_DIS_SERV_ID 0x02
457 
462 #define SNP_DEVINFO_SYSTEM_ID 0
463 #define SNP_DEVINFO_MODEL_NUMBER 1
464 #define SNP_DEVINFO_SERIAL_NUMBER 2
465 #define SNP_DEVINFO_FIRMWARE_REV 3
466 #define SNP_DEVINFO_HARDWARE_REV 4
467 #define SNP_DEVINFO_SOFTWARE_REV 5
468 #define SNP_DEVINFO_MANUFACTURER_NAME 6
469 #define SNP_DEVINFO_11073_CERT_DATA 7
470 #define SNP_DEVINFO_PNP_ID 8
471 
472 #define SNP_DEVINFO_SYSTEM_ID_LEN 8
474 
476 #define SNP_DEVINFO_PNP_ID_LEN 7
477 
479 // this is for information only, do not change it here.
480 #define SNP_DEVINFO_STRING_LEN 21
481 
486 #define SNP_GGS_DEVICE_NAME_ATT 0
487 #define SNP_GGS_APPEARANCE_ATT 1
488 #define SNP_GGS_PERI_PRIVACY_FLAG_ATT 2
489 #define SNP_GGS_RECONNCT_ADDR_ATT 3
490 #define SNP_GGS_PERI_CONN_PARAM_ATT 4
491 #define SNP_GGS_PERI_PRIVACY_FLAG_PROPS 5
492 #define SNP_GGS_W_PERMIT_DEVICE_NAME_ATT 6
493 #define SNP_GGS_W_PERMIT_APPEARANCE_ATT 7
494 #define SNP_GGS_W_PERMIT_PRIVACY_FLAG_ATT 8
495 
496 #define SNP_GAP_DEVICE_NAME_LEN 21
498 
499 // Privacy Flag States
500 #define SNP_GAP_PRIVACY_DISABLED 0x00
501 #define SNP_GAP_PRIVACY_ENABLED 0x01
502 
503 
508 #define SNP_DESC_HEADER_GEN_SHORT_UUID 0x01
509 #define SNP_DESC_HEADER_GEN_LONG_UUID 0x02
510 #define SNP_DESC_HEADER_CCCD 0x04
511 #define SNP_DESC_HEADER_FORMAT 0x08
512 #define SNP_DESC_HEADER_USER_DESC 0x80
513 #define SNP_DESC_HEADER_UNSUPPORTED_MASK 0x70
514 
516 #define SNP_GATT_CLIENT_CFG_NOTIFY 0x0001
517 #define SNP_GATT_CLIENT_CFG_INDICATE 0x0002
518 
519 
522 #define SNP_RESPONSE_NOT_NEEDED 0x00
523 #define SNP_RESPONSE_NEEDED 0x01
524 
526 #define SNP_INVALID_HANDLE 0x0000
527 
528 
532 #define SNP_GAP_TERM_CONN_DEFAULT 0x00
533 #define SNP_GAP_TERM_CONN_IMMEDIATLY 0x01
534 
539 #define SNP_GAPBOND_PAIRING_MODE 0x00
540 #define SNP_GAPBOND_IO_CAPABILITIES 0x01
541 #define SNP_GAPBOND_BONDING_ENABLED 0x02
542 #define SNP_GAPBOND_ERASE_ALLBONDS 0x03
543 #define SNP_GAPBOND_LRU_BOND_REPLACEMENT 0x04
544 
549 #define SNP_GAPBOND_PAIRING_STATE_COMPLETE 0x01
550 #define SNP_GAPBOND_PAIRING_STATE_BONDED 0x02
551 #define SNP_GAPBOND_PAIRING_STATE_BOND_SAVED 0x03
552 
556 /*-------------------------------------------------------------------
557 * TYPEDEFS - Initialization and Configuration
558 */
559 /*** Device Data Types ***/
560 
572 PACKED_TYPEDEF_STRUCT
573 {
574  uint16_t eventMask;
578 
586 PACKED_TYPEDEF_STRUCT
587 {
588  uint16_t maskedEvent;
592 
600 PACKED_TYPEDEF_STRUCT
601 {
602  uint16_t memAlo;
603  uint16_t memMax;
604  uint16_t memSize;
606 
614 PACKED_TYPEDEF_STRUCT
615 {
616  uint16_t opcode;
617  uint8_t *pData;
625 
633 PACKED_TYPEDEF_STRUCT
634 {
635  uint8_t status;
636  uint16_t opcode;
637  uint8_t *pData;
644 
652 PACKED_TYPEDEF_STRUCT
653 {
654  uint8_t status;
655  uint16_t snpVer;
656  uint8_t stackBuildVer[10];
658 
666 PACKED_TYPEDEF_STRUCT
667 {
668  uint32_t rand;
670 
676 PACKED_TYPEDEF_STRUCT
677 {
678  uint8_t gapRoleStatus;
679  uint8_t advStatus;
683  uint8_t ATTstatus;
687  uint8_t ATTmethod;
692 
693 /*** GAP Data Types ***/
694 
702 PACKED_TYPEDEF_STRUCT
703 {
704  uint8_t type;
705  uint16_t timeout;
706  uint16_t interval;
709  uint8_t filterPolicy;
713  uint8_t initiatorAddress[6];
714  uint8_t behavior;
716 
717 
727 PACKED_TYPEDEF_STRUCT
728 {
729  uint8_t type;
730  uint8_t *pData;
732 
742 PACKED_TYPEDEF_STRUCT
743 {
744  uint16_t connHandle;
745  uint8_t option;
747 
755 PACKED_TYPEDEF_STRUCT
756 {
757  uint16_t connHandle;
758  uint16_t intervalMin;
759  uint16_t intervalMax;
765  uint16_t slaveLatency;
771  uint16_t supervisionTimeout;
774 
780 
790 PACKED_TYPEDEF_STRUCT
791 {
792  uint8_t status;
793  uint16_t connHandle;
795 
829 PACKED_TYPEDEF_STRUCT
830 {
831  uint16_t paramId;
832  uint16_t value;
834 
844 PACKED_TYPEDEF_STRUCT
845 {
846  uint8_t status;
847  uint16_t paramId;
848  uint16_t value;
850 
862 PACKED_TYPEDEF_STRUCT
863 {
864  uint32_t authData;
866 
867 /*** GATT Data Types ***/
868 
876 PACKED_TYPEDEF_STRUCT
877 {
878  uint8_t type;
879  uint8_t UUID[16];
885 
906 PACKED_TYPEDEF_STRUCT
907 {
908  uint8_t charValPerms;
909  uint16_t charValProps;
910  uint8_t mgmtOption;
911  uint16_t charValMaxLen;
912  uint8_t UUID[16];
920 
928 PACKED_TYPEDEF_STRUCT
929 {
930  uint8_t status;
931  uint16_t attrHandle;
933 
948 PACKED_TYPEDEF_STRUCT
949 {
950  uint8_t perms;
952 
962 PACKED_TYPEDEF_STRUCT
963 {
964  uint8_t format;
965  uint8_t exponent;
966  uint16_t unit;
967  uint8_t namespace;
968  uint16_t desc;
970 
980 PACKED_TYPEDEF_STRUCT
981 {
982  uint8_t perms;
983  uint16_t maxLen;
984  uint16_t initLen;
985  uint8_t *pDesc;
987 
997 PACKED_TYPEDEF_STRUCT
998 {
999  uint8_t perms;
1000  uint16_t maxLen;
1001  uint8_t UUID[2];
1005 
1015 PACKED_TYPEDEF_STRUCT
1016 {
1017  uint8_t perms;
1018  uint16_t maxLen;
1019  uint8_t UUID[16];
1023 
1044 PACKED_TYPEDEF_STRUCT
1045 {
1046  uint8_t header;
1053 
1064 PACKED_TYPEDEF_STRUCT
1065 {
1066  uint8_t status;
1067  uint8_t header;
1068  uint16_t handles[6];
1073 
1081 PACKED_TYPEDEF_STRUCT
1082 {
1083  uint8_t status;
1084  uint16_t startHandle;
1085  uint16_t endHandle;
1087 
1095 PACKED_TYPEDEF_STRUCT
1096 {
1097  uint16_t connHandle;
1098  uint16_t attrHandle;
1099  uint16_t offset;
1100  uint16_t maxSize;
1102 
1110 PACKED_TYPEDEF_STRUCT
1111 {
1112  uint8_t status;
1113  uint16_t connHandle;
1114  uint16_t attrHandle;
1115  uint16_t offset;
1116  uint8_t *pData;
1119 
1129 PACKED_TYPEDEF_STRUCT
1130 {
1131  uint16_t connHandle;
1132  uint16_t attrHandle;
1133  uint8_t rspNeeded;
1134  uint16_t offset;
1135  uint8_t *pData;
1138 
1158 PACKED_TYPEDEF_STRUCT
1159 {
1160  uint8_t status;
1161  uint16_t connHandle;
1163 
1169 PACKED_TYPEDEF_STRUCT
1170 {
1171  uint16_t connHandle;
1172  uint16_t attrHandle;
1173  uint8_t authenticate;
1174  uint8_t type;
1175  uint8_t *pData;
1177 
1246 PACKED_TYPEDEF_STRUCT
1247 {
1248  uint8_t status;
1252 
1268 PACKED_TYPEDEF_STRUCT
1269 {
1270  uint8_t serviceID;
1271  uint8_t paramID;
1274  uint8_t *pData;
1276 
1284 PACKED_TYPEDEF_STRUCT
1285 {
1286  uint16_t attrHandle;
1287  uint8_t *pData;
1289 
1297 PACKED_TYPEDEF_STRUCT
1298 {
1299  uint8_t status;
1300  uint16_t attrHandle;
1302 
1310 PACKED_TYPEDEF_STRUCT
1311 {
1312  uint16_t attrHandle;
1314 
1322 PACKED_TYPEDEF_STRUCT
1323 {
1324  uint8_t status;
1325  uint16_t attrHandle;
1326  uint8_t *pData;
1328 
1336 PACKED_TYPEDEF_STRUCT
1337 {
1338  uint8_t serviceID;
1339  uint8_t paramID;
1341 
1351 PACKED_TYPEDEF_STRUCT
1352 {
1353  uint16_t connHandle;
1354  uint16_t cccdHandle;
1355  uint8_t rspNeeded;
1356  uint16_t value;
1358 
1366 PACKED_TYPEDEF_STRUCT
1367 {
1368  uint8_t useWhiteList;
1370 
1375 typedef union
1376 {
1377  //Mask events
1380 
1381  //Revision
1383 
1384  //Rand
1386 
1387  //HCI
1390 
1391  //Status
1393 
1394  //Test
1396 
1397  //Advertising
1400  snpSetAdvDataCnf_t setAdvDataCnf;
1401 
1402  //Connection
1406 
1407  //GAP Parameters
1409  snpSetGapParamRsp_t setGapParamRsp;
1410  snpGetGapParamReq_t getGapParamReq;
1412 
1413  //Security
1414  snpSetSecParamReq_t setSecParamReq;
1415  snpSetSecParamRsp_t setSecParamRsp;
1417  snpSetAuthDataRsp_t setAuthDataRsp;
1418 
1419  //White List
1421  snpSetWhiteListRsp_t setWhiteListRsp;
1422 
1423  //Services
1425  snpAddServiceRsp_t addServiceRsp;
1431 
1432  //Incoming GATT Requests
1438  snpNotifIndCnf_t notifIndCnf;
1439 
1440  //NP GATT Parameters of predefined services
1444  snpGetGattParamRsp_t getGattParamRsp;
1445 
1446  //CCCD Updates
1448  snpCharCfgUpdatedRsp_t charcfgUpdatedRsp;
1449 } snp_msg_t;
1450 
1451 /*** SNP EVENTS ***/
1452 
1462 PACKED_TYPEDEF_STRUCT
1463 {
1464  uint16_t connHandle;
1465  uint16_t connInterval;
1466  uint16_t slaveLatency;
1468  uint8_t addressType;
1469  uint8_t pAddr[6];
1470 } snpConnEstEvt_t;
1471 
1481 PACKED_TYPEDEF_STRUCT
1482 {
1483  uint16_t connHandle;
1484  uint8_t reason;
1486 
1496 PACKED_TYPEDEF_STRUCT
1497 {
1498  uint16_t connHandle;
1499  uint16_t connInterval;
1500  uint16_t slaveLatency;
1503 
1513 PACKED_TYPEDEF_STRUCT
1514 {
1515  uint8_t status;
1517 
1527 PACKED_TYPEDEF_STRUCT
1528 {
1529  uint8_t state;
1530  uint8_t status;
1532 
1542 PACKED_TYPEDEF_STRUCT
1543 {
1544  uint16_t opcode;
1545  uint8_t status;
1546 } snpErrorEvt_t;
1547 
1557 PACKED_TYPEDEF_STRUCT
1558 {
1559  uint16_t connHandle;
1560  uint16_t attMtuSize;
1562 
1572 PACKED_TYPEDEF_STRUCT
1573 {
1574  uint8_t display;
1575  uint8_t input;
1576  uint32_t numCmp;
1578 
1583 typedef union
1584 {
1593 } snpEventParam_t;
1594 
1602 PACKED_TYPEDEF_STRUCT
1603 {
1604  uint16_t event;
1606 } snpEvt_t;
1607 
1617 typedef struct
1618 {
1619  uint16_t intervalMin;
1620  uint16_t intervalMax;
1621  uint16_t latency;
1622  uint16_t timeout;
1624 
1627 /*********************************************************************
1628  * MACROS
1629  */
1630 
1635 #define SNP_CMD1_HDR_MASK 0xC0
1637 
1639 #define SNP_CMD1_HDR_POS 0x6
1640 
1642 #define SNP_GET_OPCODE_HDR_CMD1(cmd) (((cmd) & SNP_CMD1_HDR_MASK) >> SNP_CMD1_HDR_POS)
1643 
1645 #define SNP_CMD1_ID_MASK 0x3F
1646 
1648 #define SNP_GET_OPCODE_ID_CMD1(cmd) ((cmd) & SNP_CMD1_ID_MASK)
1649 
1652 /*********************************************************************
1653 *********************************************************************/
1654 
1655 #ifdef __cplusplus
1656 }
1657 #endif
1658 
1659 #endif /* SNP_H */
1660 
Parameter Structure for the ATT MTU size updated Event data.
Definition: snp.h:1557
uint16_t value
2 Byte Parameter Value set if for SET command
Definition: snp.h:832
uint16_t memAlo
2 Byte HEAP allocated memory
Definition: snp.h:602
Parameter Structure for the Error Event SNP_ERROR_EVT.
Definition: snp.h:1542
uint16_t event
2 Byte Event, list of asynchronous events generated by the SNP.
Definition: snp.h:1604
uint8_t header
1 Byte Header Field, SNP GATT Descriptors Header
Definition: snp.h:1046
Parameter Structure for SNP_updateConnParam.
Definition: snp.h:755
uint16_t maskedEvent
Definition: snp.h:588
Parameter Structure for the Security Event.
Definition: snp.h:1527
snpSetSecParamReq_t setSecParamReq
Set the Security Requirements request.
Definition: snp.h:1414
Parameter Structure for SNP_CHAR_READ_IND / @ ref SNP_charRead.
Definition: snp.h:1095
uint8_t reason
1 Byte Reason of the termination connection termination reason.
Definition: snp.h:1484
Parameter Structure for the Characteristic Configuration Update Indication.
Definition: snp.h:1351
snpSetSecParamRsp_t setSecParamRsp
Set Security Requirements response.
Definition: snp.h:1415
uint32_t authData
4 Byte Authentication Data. 000000 - 999999 or TRUE/FALSE
Definition: snp.h:864
snpRegisterServiceRsp_t registerService
Register service Response.
Definition: snp.h:1430
struct snpCharWriteCnf_t snpNotifIndCnf_t
Parameter Structure for SNP_sendNotifcnf_rsp - Same Structure as snpCharWriteCnf_t.
Connection parameters for the peripheral device.
Definition: snp.h:1617
snpErrorEvt_t advErrorEvt
Parameter Structure snpErrorEvt_t.
Definition: snp.h:1590
Parameter Structure for SNP_setGATTParam / SNP_SET_GATT_PARAM_RSP.
Definition: snp.h:1268
uint16_t charValMaxLen
Definition: snp.h:911
Parameter Structure for SNP_getGATTParam / SNP_GET_GATT_PARAM_REQ.
Definition: snp.h:1336
Parameter Structure for the Characteristic Write Request Indication data.
Definition: snp.h:1129
snpSetGapParamRsp_t setGapParamRsp
Set GAP parameter Response.
Definition: snp.h:1409
snpUpdateConnParamCnf_t updateConnParamsCnf
Update connection parameters, request.
Definition: snp.h:1405
Parameter Structure for SNP_UPDATE_CONN_PARAM_CNF.
Definition: snp.h:790
Parameter Structure for SNP_setAuthenticationData / SNP_SET_AUTHENTICATION_DATA_REQ.
Definition: snp.h:862
uint8_t useWhiteList
1 Byte White List Filter Policy, Advertisement Filter Policy Type
Definition: snp.h:1368
uint16_t attrHandle
2 Byte attribute handle of the characteristic value.
Definition: snp.h:931
uint16_t startHandle
2 Byte First attribute handle of the registered service
Definition: snp.h:1084
struct snpSetGattParamRsp_t snpAddServiceRsp_t
1 Byte Command Status Response
Parameter Structure for the Connection Established Event.
Definition: snp.h:1462
struct snpSetGattParamReq_t snpGetGattParamRsp_t
Parameter Structure for SNP_getGATTParam / SNP_GET_GATT_PARAM_RSP.
Parameter Structure for SNP_writeCharCnf / SNP_CHAR_WRITE_CNF.
Definition: snp.h:1158
uint32_t rand
32-bit Random Number generated by TRNG
Definition: snp.h:668
Parameter Structure for the Connection terminated Event.
Definition: snp.h:1481
uint16_t memSize
2 Byte total HEAP size
Definition: snp.h:604
uint16_t memMax
2 Byte maximum HEAP ever allocated since startup
Definition: snp.h:603
struct snpSetGattParamRsp_t snpSetGapParamRsp_t
1 Byte Command Status Response
snpAuthenticationEvt_t authenticationEvt
Parameter Structure snpAuthenticationEvt_t.
Definition: snp.h:1592
Parameter Structure for SNP_addDescriptionValue.
Definition: snp.h:1044
snpGetRevisionRsp_t revisionRsp
Get revision Response.
Definition: snp.h:1382
snpUpdateConnParamEvt_t updateConnParamEvt
Parameter Structure snpUpdateConnParamEvt_t.
Definition: snp.h:1587
Parameter Structure for the Advertising state change Event.
Definition: snp.h:1513
Parameter Structure used to add a generic attribute descriptor (long UUID)
Definition: snp.h:1015
uint8_t initiatorAddrType
1 Byte Initiator Address Type, Reserved for Future Use
Definition: snp.h:712
snpCharReadInd_t readInd
Characteristic read request.
Definition: snp.h:1433
Parameter Structure used to add a Format attribute.
Definition: snp.h:962
uint8_t authenticate
1 Byte Reserved for future use
Definition: snp.h:1173
uint8_t option
1 Byte Type of disconnection requested. see GAP GATT Terminate connection request option field...
Definition: snp.h:745
Parameter Structure to add new Characteristic Description Response SNP_ADD_CHAR_DESC_DECL_RSP.
Definition: snp.h:1064
Parameter Structure for MITM Authentication data to be displayed.
Definition: snp.h:1572
snpStartAdvReq_t startAdv
Start advertising request.
Definition: snp.h:1398
SNP Event Parameters.
Definition: snp.h:1583
uint8_t status
1 Byte status of the request (SUCCESS or Error, list of status generated by the SNP.)
Definition: snp.h:635
uint16_t attMtuSize
2 Byte New ATT MTU Size negotiated between GATT client and GATT server.
Definition: snp.h:1560
struct snpSetGattParamRsp_t snpSetWhiteListRsp_t
1 Byte Command Status Response
uint16_t initLen
2 Byte initial length of the string, plus one byte for null terminator (must be <= snpAddAttrUserDesc...
Definition: snp.h:984
snpAddServiceRsp_t addServiceRsp
Add service response.
Definition: snp.h:1425
snpTestCmdRsp_t testCmdRsp
Test command response.
Definition: snp.h:1395
Parameter Structure for the response to SNP_getRev.
Definition: snp.h:666
uint16_t unit
2 Byte Unit, as described by BLE Spec, Vol 3, Part G, Chapter 3.3
Definition: snp.h:966
uint16_t endHandle
2 Byte Last attribute handle of the registered service
Definition: snp.h:1085
Parameter Structure for SNP_registerService / SNP_REGISTER_SERVICE_RSP.
Definition: snp.h:1081
snpSecurityEvt_t securityEvt
Parameter Structure snpSecurityEvt_t.
Definition: snp.h:1591
uint16_t desc
< 1 Byte Namespace, as described by BLE Spec, Vol 3, Part G, Chapter 3.3
Definition: snp.h:967
uint16_t latency
2 Byte
Definition: snp.h:1621
Parameter Structure for the Update Connection Parameter Event.
Definition: snp.h:1496
snpConnTermEvt_t connTermEvt
Parameter Structure snpConnTermEvt_t.
Definition: snp.h:1586
snpATTMTUSizeEvt_t attMTUSizeEvt
Parameter Structure snpATTMTUSizeEvt_t.
Definition: snp.h:1589
uint8_t behavior
1 Byte Behavior of Advertisement on connection event, Adv. behavior when connection are established o...
Definition: snp.h:714
snpAddAttrFormat_t * pFormat
Pointer to Parameter Structure, snpAddAttrFormat_t.
Definition: snp.h:1050
snpSetGattParamRsp_t setGattParamRsp
Set GATT parameter response.
Definition: snp.h:1442
snpGetGapParamReq_t getGapParamReq
Get GAP parameter Request.
Definition: snp.h:1410
uint8_t perms
1 Byte permissions of the attribute, GATT Attribute Access Permissions Bit Fields ...
Definition: snp.h:950
Parameter Structure for SNP_CHAR_READ_CNF / snpCharReadCnf_t.
Definition: snp.h:1110
snpAddAttrUserDesc_t * pUserDesc
Pointer to Parameter Structure, snpAddAttrUserDesc_t.
Definition: snp.h:1051
snpAddAttrGenLongUUID_t * pLongUUID
Pointer to Parameter Structure, snpAddAttrGenLongUUID_t.
Definition: snp.h:1048
struct snpSetGapParamReq_t snpGetGapParamReq_t
Parameter Structure for SNP_getGapParam / SNP_GET_GAP_PARAM_REQ - Same Structure as snpSetGapParamReq...
struct snpCharWriteCnf_t snpCharCfgUpdatedRsp_t
Parameter Structure for SNP_processCharConfigUpdatedCnf / SNP_CCCD_UPDATED_CNF - Same Structure as sn...
snpGetStatusCmdRsp_t getStatusRsp
Get status Response.
Definition: snp.h:1392
snpUpdateConnParamReq_t updateConnParamsReq
Update connection parameters indication.
Definition: snp.h:1404
uint16_t maxSize
2 Byte Max Size of the data to read
Definition: snp.h:1100
uint8_t gapRoleStatus
1 Byte Current state of the GAP Role ( gaprole_States_t)
Definition: snp.h:678
snpCharCfgUpdatedRsp_t charcfgUpdatedRsp
Characteristic configuration update response.
Definition: snp.h:1448
uint16_t snpVer
2 Byte Version of the SNP (major, minor)
Definition: snp.h:655
Parameter Structure used for SNP_addCharValueDecl / SNP_ADD_CHAR_VAL_DECL_REQ.
Definition: snp.h:906
uint8_t charValPerms
1 Byte permissions of the value attribute, see GATT Attribute Access Permissions Bit Fields ...
Definition: snp.h:908
1 Byte Command Status Response
Definition: snp.h:1246
snpAddCharDescDeclRsp_t addCharDescDeclRsp
Add characteristic descriptor Response.
Definition: snp.h:1429
uint16_t supervisionTimeout
2 Byte
Definition: snp.h:1467
uint16_t connHandle
2 Byte Connection Handle to terminate
Definition: snp.h:744
snpCharWriteCnf_t charWriteCnf
Characteristic write confirmation.
Definition: snp.h:1436
snpNotifIndReq_t notifIndReq
Notification or indication request.
Definition: snp.h:1437
struct snpSetGapParamReq_t snpSetSecParamReq_t
Parameter Structure for SNP_setSecurityParams / SNP_SET_SECURITY_PARAM_REQ - Same Structure as snpSet...
Parameter Structure used to add a Client Characteristic Configuration Description Attribute...
Definition: snp.h:948
snpSetAdvDataCnf_t setAdvDataCnf
Set advertising data Response.
Definition: snp.h:1400
uint8_t type
1 Byte Type of Advertisement, see Advertisement Type
Definition: snp.h:704
uint8_t addressType
1 Byte Type of initiator address
Definition: snp.h:1468
uint8_t input
1 Byte TRUE if device must input passcode.
Definition: snp.h:1575
snpCharReadCnf_t readCnf
Characteristic read confirmation.
Definition: snp.h:1434
snpAddCharValueDeclRsp_t addCharValueDecRsp
Add characteristic value Response.
Definition: snp.h:1427
SNP_CMD1_HDR_TYPE
list of subgroup
Definition: snp.h:72
uint8_t * pData
Definition: snp.h:637
snpHciCmdRsp_t hciCmdRsp
HCI command response (event)
Definition: snp.h:1389
Add Service Request Structure for SNP_addService / SNP_ADD_SERVICE_REQ.
Definition: snp.h:876
Parameter Structure for SNP_maskEvt.
Definition: snp.h:572
Parameter Structure for SNP_setWhiteListFilterPolicy / SNP_SET_WHITE_LIST_POLICY_REQ.
Definition: snp.h:1366
uint16_t timeout
2 Byte Timeout of the advertisement.
Definition: snp.h:705
Parameter Structure for SNP_MASK_EVENT_RSP.
Definition: snp.h:586
uint8_t state
1 Byte New Security State Security States
Definition: snp.h:1529
struct snpSetGattParamRsp_t snpSetAuthDataRsp_t
1 Byte Command Status Response
Parameter Structure for Response to SNP_addCharValueDecl / SNP_ADD_CHAR_VAL_DECL_RSP.
Definition: snp.h:928
struct snpSetGattParamRsp_t snpSetSecParamRsp_t
1 Byte Command Status Response
snpAddCharValueDeclReq_t addCharValueDecReq
Add characteristic value Request.
Definition: snp.h:1426
uint16_t offset
2 Byte Offset of the characteristic to start reading from
Definition: snp.h:1099
snpSetGattParamReq_t setGattParamReq
Set GATT parameter request.
Definition: snp.h:1441
Parameter Structure used to add a generic attribute descriptor (short UUID)
Definition: snp.h:997
snpCharCfgUpdatedInd_t charCfgUpdatedReq
Characteristic configuration updated indication.
Definition: snp.h:1447
snpGetGattParamReq_t getGattParamReq
Get GATT parameter response.
Definition: snp.h:1443
Parameter Structure for the Characteristic Notification and Indication Request data This is a packed ...
Definition: snp.h:1169
uint16_t intervalMin
2 Byte Minimum value for the connection event interval.
Definition: snp.h:758
snpAddServiceReq_t addServiceReq
Add service request.
Definition: snp.h:1424
snpSetAuthDataReq_t setAuthDataReq
Set Authentication Data request.
Definition: snp.h:1416
snpEventParam_t * pEvtParams
snpEventParam_t
Definition: snp.h:1605
uint16_t charValProps
2 Byte property of the value attribute, see GATT Characteristic Properties Bit Fields ...
Definition: snp.h:909
Parameter Structure for SNP_setGapParam / SNP_SET_GAP_PARAM_REQ.
Definition: snp.h:829
snpAddAttrCccd_t * pCCCD
Pointer to Parameter Structure, snpAddAttrCccd_t.
Definition: snp.h:1049
uint8_t paramID
1 Byte ID of the parameter to retrieved.
Definition: snp.h:1339
snpMaskEventRsp_t maskEventCnf
event mask confirmation.
Definition: snp.h:1379
uint16_t connInterval
2 Byte
Definition: snp.h:1465
snpSetAuthDataRsp_t setAuthDataRsp
Set Authentication Data response.
Definition: snp.h:1417
snpHciCmdReq_t hciCmdReq
HCI command request.
Definition: snp.h:1388
Connection Termination Request Structure.
Definition: snp.h:742
uint16_t intervalMax
2 Byte
Definition: snp.h:1620
snpNotifIndCnf_t notifIndCnf
Indication Confirmation.
Definition: snp.h:1438
uint16_t cccdHandle
2 Byte Handle of the characteristic value attribute to notify/indicate
Definition: snp.h:1354
snpSetWhiteListRsp_t setWhiteListRsp
Set the White List Filter Policy response.
Definition: snp.h:1421
uint16_t opcode
Definition: snp.h:616
SNP Event Structure.
Definition: snp.h:1602
Parameter Structure for the Get GAP Parameter Value Response.
Definition: snp.h:844
Parameter Structure for SNP_getAttrValue / SNP_SET_ATTR_VALUE_REQ.
Definition: snp.h:1310
uint16_t eventMask
Definition: snp.h:574
snpSetGapParamReq_t setGapParamReq
Set GAP parameter Request.
Definition: snp.h:1408
Parameter Structure for response to SNP_setAttrValue / SNP_SET_ATTR_VALUE_RSP.
Definition: snp.h:1297
snpAdvStatusEvt_t advStatusEvt
Parameter Structure snpAdvStatusEvt_t.
Definition: snp.h:1588
uint32_t numCmp
32 bit Numeric Comparison value to display, 0 if not used.
Definition: snp.h:1576
The SNP message. A union of all SNP message types.
Definition: snp.h:1375
snpSetAdvDataReq_t setAdvDataReq
Set advertising data Request.
Definition: snp.h:1399
uint16_t slaveLatency
2 Byte
Definition: snp.h:1466
snpGetGapParamRsp_t getGapParamRsp
Get GAP parameter Response.
Definition: snp.h:1411
struct snpSetGattParamRsp_t snpSetAdvDataCnf_t
1 Byte Command Status Response
snpTermConnReq_t connTermReq
Connection terminated Request.
Definition: snp.h:1403
Parameter Structure for SNP_startAdv.
Definition: snp.h:702
Parameter Structure for SNP_getRev.
Definition: snp.h:652
uint16_t paramId
2 Byte GAP Parameter ID, GAP Parameter IDs or snpSetSecParamReq_t
Definition: snp.h:831
snpCharWriteInd_t charWriteInd
Characteristic write request.
Definition: snp.h:1435
uint16_t maxLen
2 Byte Maximum possible length of the string, plus one byte for null terminator (range from 1 to 512)...
Definition: snp.h:983
uint8_t display
1 Byte TRUE if device must display passcode.
Definition: snp.h:1574
Parameter Structure for response to SNP_getAttrValue / SNP_SET_ATTR_VALUE_RSP.
Definition: snp.h:1322
Parameter Structure for SNP_setAttrValue / SNP_SET_ATTR_VALUE_REQ.
Definition: snp.h:1284
Parameter Structure for SNP_HCI_CMD_RSP.
Definition: snp.h:633
uint8_t * pDesc
Pointer to initial string (must be null terminated)
Definition: snp.h:985
Parameter Structure for the response to SNP_getStatus This is a packed structure. see Dealing with Pa...
Definition: snp.h:676
Parameter Structure for SNP_setAdvData.
Definition: snp.h:727
snpGetGattParamRsp_t getGattParamRsp
Get GATT parameter request.
Definition: snp.h:1444
uint8_t exponent
1 Byte Exponent, as described by BLE Spec, Vol 3, Part G, Chapter 3.3
Definition: snp.h:965
uint8_t mgmtOption
1 Byte Reserved for future use
Definition: snp.h:910
snpGetRandRsp_t randRsp
Get Random Number Response.
Definition: snp.h:1385
snpConnEstEvt_t connEstEvt
Parameter Structure snpConnEstEvt_t.
Definition: snp.h:1585
snpAddCharDescDeclReq_t addCharDescDeclReq
Add characteristic descriptor Request.
Definition: snp.h:1428
uint8_t rspNeeded
1 Byte Indicate if the AP must answer this indication or not, Options for Response Needed Field ...
Definition: snp.h:1133
Parameter Structure used to add a User Descriptor attribute.
Definition: snp.h:980
snpAddAttrGenShortUUID_t * pShortUUID
Pointer to Parameter Structure, snpAddAttrGenShortUUID_t.
Definition: snp.h:1047
uint8_t serviceID
Definition: snp.h:1270
Parameter Structure for SNP_executeHCIcmd.
Definition: snp.h:614
snpMaskEventReq_t maskEventReq
event mask request.
Definition: snp.h:1378
uint8_t format
1 Byte Format, as described by BLE Spec, Vol 3, Part G, Chapter 3.3
Definition: snp.h:964
Parameter Structure for SNP_executeTestCmd.
Definition: snp.h:600
snpSetWhiteListReq_t setWhiteListReq
Set the White List Filter Policy request.
Definition: snp.h:1420
© Copyright 1995-2019, Texas Instruments Incorporated. All rights reserved.
Trademarks | Privacy policy | Terms of use | Terms of sale