Radio Control Layer (RCL)
|
#include <stdint.h>
#include <stddef.h>
#include <ti/drivers/rcl/RCL_Command.h>
#include <ti/drivers/rcl/hal/hal.h>
Go to the source code of this file.
Data Structures | |
struct | RCL_SchedulerStopInfo |
struct | RCL_SchedulerState |
Macros | |
#define | RCL_SCHEDULER_SYSTIM_US(x) (((uint32_t) (x)) * 4U) |
#define | RCL_SCHEDULER_SYSTIM_MS(x) (((uint32_t) (x)) * 4U * 1000U) |
#define | ABS_START_TIME_OFFSET RCL_SCHEDULER_SYSTIM_US(100U) |
#define | IMM_START_TIME_OFFSET RCL_SCHEDULER_SYSTIM_US(90U) |
#define | RCL_SCHEDULER_MARGIN_ARM RCL_SCHEDULER_SYSTIM_US(40U) |
#define | RCL_SCHEDULER_MARGIN_CONFIGURE RCL_SCHEDULER_SYSTIM_US(76U) |
#define | RCL_SCHEDULER_MARGIN_LOAD RCL_SCHEDULER_SYSTIM_US(460U) |
#define | RCL_SCHEDULER_SLEEP_CUTOFF RCL_SCHEDULER_SYSTIM_MS(10U) |
#define | RCL_SCHEDULER_TRIG_NOW_DELAY RCL_SCHEDULER_SYSTIM_US(50U) |
#define | RCL_SCHEDULER_WAKEUP_MARGIN RCL_SCHEDULER_SYSTIM_US(1000U) |
Enumerations | |
enum | RCL_SchedulerStopTimeSelect { RCL_SchedulerStopTimeSelect_None = 0, RCL_SchedulerStopTimeSelect_Cmd = 1, RCL_SchedulerStopTimeSelect_Sched = 2 } |
enum | RCL_SchedulerStopTimeState { RCL_SchedulerStopTimeState_Init = 0, RCL_SchedulerStopTimeState_Found = 1, RCL_SchedulerStopTimeState_Programmed = 2 } |
Functions | |
RCL_CommandStatus | RCL_Scheduler_setStartStopTime (const RCL_Command *cmd) |
Set start and stop time for LRF based on command. More... | |
RCL_CommandStatus | RCL_Scheduler_setStartStopTimeEarliestStart (const RCL_Command *cmd, uint32_t earliestStartTime) |
Set start and stop time for LRF based on command with earliest start time. More... | |
RCL_CommandStatus | RCL_Scheduler_setCmdStopTimeNoStartTrigger (const RCL_Command *cmd) |
Set stop time for LRF based on command when it does not need a start trigger. More... | |
RCL_CommandStatus | RCL_Scheduler_setNewStartNow (void) |
Set new start time for LRF to now, after a previous start. More... | |
RCL_CommandStatus | RCL_Scheduler_setNewStartAbsTime (uint32_t startTime) |
Set new start time for LRF to given absolute time, after a previous start. More... | |
RCL_CommandStatus | RCL_Scheduler_setNewStartRelTime (uint32_t relStartTime) |
Set new start time for LRF to given time relative to previous LRF start. More... | |
RCL_StopType | RCL_Scheduler_setStopTimes (void) |
Function to apply relevant stop times. More... | |
bool | RCL_Scheduler_isLater (uint32_t refTime, uint32_t chkTime) |
Find if a time instant occurs after another, allowing wrap-around. More... | |
int32_t | RCL_Scheduler_delta (uint32_t refTime, uint32_t chkTime) |
Find the time difference between two times, allowing wrap-around. More... | |
static uint32_t | RCL_Scheduler_getCurrentTime (void) |
Get current time. More... | |
RCL_StopType | RCL_Scheduler_setSchedStopTime (RCL_SchedulerStopInfo *stopInfo, uint32_t schedStopTime) |
Set scheduler stop time. More... | |
bool | RCL_Scheduler_postEvent (RCL_Command_Handle c, RCL_Events e) |
Post event to command handler. More... | |
Variables | |
RCL_SchedulerState | rclSchedulerState |
struct RCL_SchedulerStopInfo |
Data Fields | ||
---|---|---|
uint32_t | cmdStopEnabled: 1 | |
uint32_t | schedStopEnabled: 1 | |
uint32_t | apiStopEnabled: 1 | |
RCL_SchedulerStopTimeSelect | stopTimeSelect: 2 | |
uint32_t | cmdStopTime | |
uint32_t | schedStopTime |
struct RCL_SchedulerState |
Data Fields | ||
---|---|---|
RCL_Command * | currCmd | |
uint32_t | nextWantsStop: 1 | |
RCL_SchedulerStopTimeState | stopTimeState: 2 | |
RCL_Events | postedRclEvents | |
uint32_t | actualStartTime | |
RCL_SchedulerStopInfo | hardStopInfo | |
RCL_SchedulerStopInfo | gracefulStopInfo |
#define RCL_SCHEDULER_SYSTIM_US | ( | x | ) | (((uint32_t) (x)) * 4U) |
Number of ticks in the given number of microseconds
#define RCL_SCHEDULER_SYSTIM_MS | ( | x | ) | (((uint32_t) (x)) * 4U * 1000U) |
Number of ticks in the given number of milliseconds
#define ABS_START_TIME_OFFSET RCL_SCHEDULER_SYSTIM_US(100U) |
Delay from scheduled start to start trigger to LRF
#define IMM_START_TIME_OFFSET RCL_SCHEDULER_SYSTIM_US(90U) |
Delay from immediate start to start trigger to LRF
#define RCL_SCHEDULER_MARGIN_ARM RCL_SCHEDULER_SYSTIM_US(40U) |
Time to prepare FIFO + PBE
#define RCL_SCHEDULER_MARGIN_CONFIGURE RCL_SCHEDULER_SYSTIM_US(76U) |
Time to reload REGBANKs
#define RCL_SCHEDULER_MARGIN_LOAD RCL_SCHEDULER_SYSTIM_US(460U) |
Time to load TOPsm images
#define RCL_SCHEDULER_SLEEP_CUTOFF RCL_SCHEDULER_SYSTIM_MS(10U) |
Time margin when not to arm LRF immediately
#define RCL_SCHEDULER_TRIG_NOW_DELAY RCL_SCHEDULER_SYSTIM_US(50U) |
Delay to add to current time to allow start to be in the future
#define RCL_SCHEDULER_WAKEUP_MARGIN RCL_SCHEDULER_SYSTIM_US(1000U) |
Wakeup margin to allow for varying command and setup time
RCL_SchedulerState rclSchedulerState |
Referenced by RCL_BLE5_updateFilterList(), RCL_Command_stop(), RCL_Command_submit(), RCL_Handler_BLE5_adv(), RCL_Handler_BLE5_conn(), RCL_Handler_BLE5_genericRx(), RCL_Handler_BLE5_scan_init(), RCL_Handler_Generic_Rx(), RCL_Handler_Generic_TxRepeat(), RCL_Handler_Nesb_Prx(), RCL_Handler_Nesb_Ptx(), RCL_Lite_Command_isFinished(), RCL_Lite_Command_start(), RCL_Lite_Command_stop(), RCL_Lite_CommandHwi(), RCL_MultiBuffer_put(), RCL_Scheduler_postEvent(), RCL_Scheduler_setNewStartRelTime(), RCL_Scheduler_setSchedStopTime(), RCL_Scheduler_setStopTimes(), RCL_TxBuffer_put(), rclCommandHwi(), rclDispatchHwi(), rclPowerNotify(), rclSchedulerHwi(), and rclSchedulerProcessCmdStartStopTime().