TI-RTOS Drivers  tidrivers_cc13xx_cc26xx_2_21_00_04
Data Structures | Macros | Typedefs | Enumerations | Functions
ADCBuf.h File Reference

Detailed Description

ADCBuf driver interface.

============================================================================

The ADCBuf header file should be included in an application as follows:

Operation

The ADCBuf driver in TI-RTOS samples an analogue waveform at a specified frequency. The resulting samples are transferred to a buffer provided by the application. The driver can either take n samples once, or continuously sample by double-buffering and providing a callback to process each finished buffer.

The APIs in this driver serve as an interface to a typical TI-RTOS application. The specific peripheral implementations are responsible to create all the SYS/BIOS specific primitives to allow for thread-safe operation.

Opening the driver

ADCBuf_Handle adcBufHandle;
ADCBuf_Params adcBufParams;
ADCBuf_Params_init(&adcBufParams);
adcBufHandle = ADCBuf_open(Board_ADCBuf0, &adcBufParams);

Making a conversion

In this context, a conversion refers to taking multiple ADC samples and transferring them to an application-provided buffer. To start a conversion, the application must configure an ADCBuf_Conversion struct and call ADCBuf_convert(). In blocking mode, ADCBuf_convert() will return when the conversion is finished and the desired number of samples have been made. In callback mode, ADCBuf_convert() will return immediately and the application will get a callback when the conversion is done.

ADCBuf_Conversion blockingConversion;
blockingConversion.arg = NULL;
blockingConversion.adcChannel = Board_ADCCHANNEL_A1;
blockingConversion.sampleBuffer = sampleBufferOnePtr;
blockingConversion.sampleBufferTwo = NULL;
blockingConversion.samplesRequestedCount = ADCBUFFERSIZE;
if (!ADCBuf_convert(adcBuf, &continuousConversion, 1)) {
// handle error
}

Canceling a conversion

ADCBuf_convertCancel() is used to cancel an ADCBuf conversion when the driver is used in ADCBuf_RETURN_MODE_CALLBACK.

Calling this API while no conversion is in progress has no effect. If a conversion is in progress, it is canceled and the provided callback function is called.

In ADCBuf_RECURRENCE_MODE_CONTINUOUS, this function must be called to stop the conversion. The driver will continue providing callbacks with fresh samples until thie ADCBuf_convertCancel() function is called. The callback function is not called after ADCBuf_convertCancel() while in ADCBuf_RECURRENCE_MODE_CONTINUOUS.

Implementation

This module serves as the main interface for TI-RTOS applications. Its purpose is to redirect the module's APIs to specific peripheral implementations which are specified using a pointer to an ADCBuf_FxnTable.

The ADCBuf driver interface module is joined (at link time) to a NULL-terminated array of ADCBuf_Config data structures named ADCBuf_config. ADCBuf_config is implemented in the application with each entry being an instance of an ADCBuf peripheral. Each entry in ADCBuf_config contains a:

Instrumentation

The ADCBuf driver interface produces log statements if instrumentation is enabled.

Diagnostics Mask Log details
Diags_USER1 basic operations performed
Diags_USER2 detailed operations performed

#include <stdint.h>
#include <stdbool.h>
#include <stddef.h>
Include dependency graph for ADCBuf.h:
This graph shows which files directly or indirectly include this file:

Go to the source code of this file.

Data Structures

struct  ADCBuf_Conversion
 An ADCBuf_Conversion data structure is used with ADCBuf_convert(). It indicates which channel to perform the ADC conversion on, how many conversions to make, and where to put them. The arg variable is an user-definable argument which gets passed to the ADCBuf_Callback when the ADC driver is in ADCBuf_RETURN_MODE_CALLBACK. More...
 
struct  ADCBuf_Params
 ADC Parameters. More...
 
struct  ADCBuf_FxnTable
 The definition of an ADCBuf function table that contains the required set of functions to control a specific ADC driver implementation. More...
 
struct  ADCBuf_Config
 ADCBuf Global configuration. More...
 

Macros

#define ADCBuf_CMD_RESERVED   32
 
#define ADCBuf_STATUS_RESERVED   -32
 
#define ADCBuf_STATUS_SUCCESS   0
 Success status code returned by: ADCBuf_control() More...
 
#define ADCBuf_STATUS_ERROR   -1
 Generic error status code returned by ADCBuf_control(). More...
 
#define ADCBuf_STATUS_UNDEFINEDCMD   -2
 An error status code returned by ADCBuf_control() for undefined command codes. More...
 

Typedefs

typedef struct ADCBuf_ConfigADCBuf_Handle
 A handle that is returned from an ADCBuf_open() call. More...
 
typedef struct ADCBuf_Conversion ADCBuf_Conversion
 An ADCBuf_Conversion data structure is used with ADCBuf_convert(). It indicates which channel to perform the ADC conversion on, how many conversions to make, and where to put them. The arg variable is an user-definable argument which gets passed to the ADCBuf_Callback when the ADC driver is in ADCBuf_RETURN_MODE_CALLBACK. More...
 
typedef void(* ADCBuf_Callback) (ADCBuf_Handle handle, ADCBuf_Conversion *conversion, void *completedADCBuffer, uint32_t completedChannel)
 The definition of a callback function used by the ADC driver when used in ADCBuf_RETURN_MODE_CALLBACK. It is called in a HWI or SWI context depending on the device specific implementation. More...
 
typedef enum ADCBuf_Recurrence_Mode ADCBuf_Recurrence_Mode
 ADC trigger mode settings. More...
 
typedef enum ADCBuf_Return_Mode ADCBuf_Return_Mode
 ADC return mode settings. More...
 
typedef struct ADCBuf_Params ADCBuf_Params
 ADC Parameters. More...
 
typedef void(* ADCBuf_CloseFxn) (ADCBuf_Handle handle)
 A function pointer to a driver specific implementation of ADCBuf_close(). More...
 
typedef ADCBuf_Handle(* ADCBuf_OpenFxn) (ADCBuf_Handle handle, ADCBuf_Params *params)
 A function pointer to a driver specific implementation of ADCBuf_open(). More...
 
typedef int_fast16_t(* ADCBuf_ControlFxn) (ADCBuf_Handle handle, uint_fast8_t cmd, void *arg)
 A function pointer to a driver specific implementation of ADCBuf_control(). More...
 
typedef void(* ADCBuf_InitFxn) (ADCBuf_Handle handle)
 A function pointer to a driver specific implementation of ADCBuf_init(). More...
 
typedef int_fast16_t(* ADCBuf_ConvertFxn) (ADCBuf_Handle handle, ADCBuf_Conversion conversions[], uint_fast8_t channelCount)
 A function pointer to a driver specific implementation of ADCBuf_convert(). More...
 
typedef int_fast16_t(* ADCBuf_ConvertCancelFxn) (ADCBuf_Handle handle)
 A function pointer to a driver specific implementation of ADCBuf_convertCancel(). More...
 
typedef uint_fast8_t(* ADCBuf_GetResolutionFxn) (ADCBuf_Handle handle)
 A function pointer to a driver specific implementation of ADCBuf_GetResolution();. More...
 
typedef int_fast16_t(* ADCBuf_adjustRawValuesFxn) (ADCBuf_Handle handle, void *sampleBuffer, uint_fast16_t sampleCount, uint32_t adcChannel)
 A function pointer to a driver specific implementation of ADCBuf_adjustRawValues();. More...
 
typedef int_fast16_t(* ADCBuf_convertAdjustedToMicroVoltsFxn) (ADCBuf_Handle handle, uint32_t adcChannel, void *adjustedSampleBuffer, uint32_t outputMicroVoltBuffer[], uint_fast16_t sampleCount)
 A function pointer to a driver specific implementation of ADCBuf_convertAdjustedToMicroVolts();. More...
 
typedef struct ADCBuf_FxnTable ADCBuf_FxnTable
 The definition of an ADCBuf function table that contains the required set of functions to control a specific ADC driver implementation. More...
 
typedef struct ADCBuf_Config ADCBuf_Config
 ADCBuf Global configuration. More...
 

Enumerations

enum  ADCBuf_Recurrence_Mode {
  ADCBuf_RECURRENCE_MODE_ONE_SHOT,
  ADCBuf_RECURRENCE_MODE_CONTINUOUS
}
 ADC trigger mode settings. More...
 
enum  ADCBuf_Return_Mode {
  ADCBuf_RETURN_MODE_BLOCKING,
  ADCBuf_RETURN_MODE_CALLBACK
}
 ADC return mode settings. More...
 

Functions

void ADCBuf_close (ADCBuf_Handle handle)
 Function to close an ADC peripheral specified by the ADC handle. More...
 
int_fast16_t ADCBuf_control (ADCBuf_Handle handle, uint_fast8_t cmd, void *arg)
 Function performs implementation specific features on a given ADCBuf_Handle. More...
 
void ADCBuf_init (void)
 This function initializes the ADC module. This function must. More...
 
void ADCBuf_Params_init (ADCBuf_Params *params)
 This function sets all fields of a specified ADCBuf_Params structure to their default values. More...
 
ADCBuf_Handle ADCBuf_open (uint_fast8_t index, ADCBuf_Params *params)
 This function opens a given ADCBuf peripheral. More...
 
int_fast16_t ADCBuf_convert (ADCBuf_Handle handle, ADCBuf_Conversion conversions[], uint_fast8_t channelCount)
 This function starts a set of conversions on one or more channels. More...
 
int_fast16_t ADCBuf_convertCancel (ADCBuf_Handle handle)
 This function cancels an ADC conversion that is in progress. More...
 
uint_fast8_t ADCBuf_getResolution (ADCBuf_Handle handle)
 This function returns the resolution in bits of the specified ADC. More...
 
int_fast16_t ADCBuf_adjustRawValues (ADCBuf_Handle handle, void *sampleBuffer, uint_fast16_t sampleCount, uint32_t adcChannel)
 This function adjusts a raw ADC output buffer such that the result is comparable between devices of the same make. The function does the adjustment in-place. More...
 
int_fast16_t ADCBuf_convertAdjustedToMicroVolts (ADCBuf_Handle handle, uint32_t adcChannel, void *adjustedSampleBuffer, uint32_t outputMicroVoltBuffer[], uint_fast16_t sampleCount)
 This function converts a raw ADC output value to a value scaled in micro volts. More...
 

Macro Definition Documentation

#define ADCBuf_CMD_RESERVED   32

Common ADCBuf_control command code reservation offset. ADC driver implementations should offset command codes with ADCBuf_CMD_RESERVED growing positively

Example implementation specific command codes:

1 #define ADCXYZ_COMMAND0 ADCBuf_CMD_RESERVED + 0
2 #define ADCXYZ_COMMAND1 ADCBuf_CMD_RESERVED + 1
#define ADCBuf_STATUS_RESERVED   -32

Common ADCBuf_control status code reservation offset. ADC driver implementations should offset status codes with ADCBuf_STATUS_RESERVED growing negatively.

Example implementation specific status codes:

1 #define ADCXYZ_STATUS_ERROR0 ADCBuf_STATUS_RESERVED - 0
2 #define ADCXYZ_STATUS_ERROR1 ADCBuf_STATUS_RESERVED - 1
3 #define ADCXYZ_STATUS_ERROR2 ADCBuf_STATUS_RESERVED - 2
#define ADCBuf_STATUS_SUCCESS   0

Success status code returned by: ADCBuf_control()

Functions return ADCBuf_STATUS_SUCCESS if the call was executed successfully.

#define ADCBuf_STATUS_ERROR   -1

Generic error status code returned by ADCBuf_control().

ADCBuf_control() returns ADCBuf_STATUS_ERROR if the control code was not executed successfully.

#define ADCBuf_STATUS_UNDEFINEDCMD   -2

An error status code returned by ADCBuf_control() for undefined command codes.

ADCBuf_control() returns ADCBuf_STATUS_UNDEFINEDCMD if the control code is not recognized by the driver implementation.

Typedef Documentation

typedef struct ADCBuf_Config* ADCBuf_Handle

A handle that is returned from an ADCBuf_open() call.

An ADCBuf_Conversion data structure is used with ADCBuf_convert(). It indicates which channel to perform the ADC conversion on, how many conversions to make, and where to put them. The arg variable is an user-definable argument which gets passed to the ADCBuf_Callback when the ADC driver is in ADCBuf_RETURN_MODE_CALLBACK.

typedef void(* ADCBuf_Callback) (ADCBuf_Handle handle, ADCBuf_Conversion *conversion, void *completedADCBuffer, uint32_t completedChannel)

The definition of a callback function used by the ADC driver when used in ADCBuf_RETURN_MODE_CALLBACK. It is called in a HWI or SWI context depending on the device specific implementation.

ADC trigger mode settings.

This enum defines if the driver should make n conversions and return or run indefinitely and run a callback function every n conversions.

ADC return mode settings.

This enum defines how the ADCBuf_convert() function returns. It either blocks or returns immediately and calls a callback function when the provided buffer has been filled.

typedef struct ADCBuf_Params ADCBuf_Params

ADC Parameters.

ADC Parameters are used to with the ADCBuf_open() call. Default values for these parameters are set using ADCBuf_Params_init().

See also
ADCBuf_Params_init()
typedef void(* ADCBuf_CloseFxn) (ADCBuf_Handle handle)

A function pointer to a driver specific implementation of ADCBuf_close().

typedef ADCBuf_Handle(* ADCBuf_OpenFxn) (ADCBuf_Handle handle, ADCBuf_Params *params)

A function pointer to a driver specific implementation of ADCBuf_open().

typedef int_fast16_t(* ADCBuf_ControlFxn) (ADCBuf_Handle handle, uint_fast8_t cmd, void *arg)

A function pointer to a driver specific implementation of ADCBuf_control().

typedef void(* ADCBuf_InitFxn) (ADCBuf_Handle handle)

A function pointer to a driver specific implementation of ADCBuf_init().

typedef int_fast16_t(* ADCBuf_ConvertFxn) (ADCBuf_Handle handle, ADCBuf_Conversion conversions[], uint_fast8_t channelCount)

A function pointer to a driver specific implementation of ADCBuf_convert().

typedef int_fast16_t(* ADCBuf_ConvertCancelFxn) (ADCBuf_Handle handle)

A function pointer to a driver specific implementation of ADCBuf_convertCancel().

typedef uint_fast8_t(* ADCBuf_GetResolutionFxn) (ADCBuf_Handle handle)

A function pointer to a driver specific implementation of ADCBuf_GetResolution();.

typedef int_fast16_t(* ADCBuf_adjustRawValuesFxn) (ADCBuf_Handle handle, void *sampleBuffer, uint_fast16_t sampleCount, uint32_t adcChannel)

A function pointer to a driver specific implementation of ADCBuf_adjustRawValues();.

typedef int_fast16_t(* ADCBuf_convertAdjustedToMicroVoltsFxn) (ADCBuf_Handle handle, uint32_t adcChannel, void *adjustedSampleBuffer, uint32_t outputMicroVoltBuffer[], uint_fast16_t sampleCount)

A function pointer to a driver specific implementation of ADCBuf_convertAdjustedToMicroVolts();.

The definition of an ADCBuf function table that contains the required set of functions to control a specific ADC driver implementation.

typedef struct ADCBuf_Config ADCBuf_Config

ADCBuf Global configuration.

The ADCBuf_Config structure contains a set of pointers used to characterise the ADC driver implementation.

This structure needs to be defined before calling ADCBuf_init() and it must not be changed thereafter.

See also
ADCBuf_init()

Enumeration Type Documentation

ADC trigger mode settings.

This enum defines if the driver should make n conversions and return or run indefinitely and run a callback function every n conversions.

Enumerator
ADCBuf_RECURRENCE_MODE_ONE_SHOT 

The driver makes n measurements and returns or runs a callback function depending on the ADCBuf_Return_Mode setting.

ADCBuf_RECURRENCE_MODE_CONTINUOUS 

The driver makes n measurements and then runs a callback function. This process happens until the application calls ADCBuf_ConvertCancelFxn(). This setting can only be used in ADCBuf_RETURN_MODE_CALLBACK.

ADC return mode settings.

This enum defines how the ADCBuf_convert() function returns. It either blocks or returns immediately and calls a callback function when the provided buffer has been filled.

Enumerator
ADCBuf_RETURN_MODE_BLOCKING 

Uses a semaphore to block while ADC conversions are performed. Context of the call must be a Task.

Note
Blocking return mode cannot be used in combination with ADCBuf_RECURRENCE_MODE_CONTINUOUS
ADCBuf_RETURN_MODE_CALLBACK 

Non-blocking and will return immediately. When the conversion is finished the configured callback function is called.

Function Documentation

void ADCBuf_close ( ADCBuf_Handle  handle)

Function to close an ADC peripheral specified by the ADC handle.

Precondition
ADCBuf_open() has to be called first.
In ADCBuf_RECURRENCE_MODE_CONTINUOUS, the application must call ADCBuf_convertCancel() first.
Parameters
handleAn ADCBuf handle returned from ADCBuf_open()
See also
ADCBuf_open()
int_fast16_t ADCBuf_control ( ADCBuf_Handle  handle,
uint_fast8_t  cmd,
void *  arg 
)

Function performs implementation specific features on a given ADCBuf_Handle.

Precondition
ADCBuf_open() has to be called first.
Parameters
handleAn ADCBuf handle returned from ADCBuf_open()
cmdA command value defined by the driver specific implementation
argA pointer to an optional R/W (read/write) argument that is accompanied with cmd
Returns
An ADCBuf_Status describing an error or success state. Negative values indicates an error.
See also
ADCBuf_open()
void ADCBuf_init ( void  )

This function initializes the ADC module. This function must.

Precondition
The ADCBuf_Config structure must exist and be persistent before this function can be called. This function call does not modify any peripheral registers. Function should only be called once.
void ADCBuf_Params_init ( ADCBuf_Params params)

This function sets all fields of a specified ADCBuf_Params structure to their default values.

Parameters
paramsA pointer to ADCBuf_Params structure for initialization

Default values are: returnMode = ADCBuf_RETURN_MODE_BLOCKING, blockingTimeout = 25000, callbackFxn = NULL, recurrenceMode = ADCBuf_RECURRENCE_MODE_ONE_SHOT, samplingFrequency = 10000, custom = NULL

ADCBuf_Params::blockingTimeout should be set large enough to allow for the desired number of samples to be collected with the specified frequency.

ADCBuf_Handle ADCBuf_open ( uint_fast8_t  index,
ADCBuf_Params params 
)

This function opens a given ADCBuf peripheral.

Parameters
indexLogical peripheral number for the ADCBuf indexed into the ADCBuf_config table
paramsPointer to an parameter block, if NULL it will use default values.
Returns
An ADCBuf_Handle on success or a NULL on an error or if it has been opened already. If NULL is returned further ADC API calls will result in undefined behaviour.
See also
ADCBuf_close()
int_fast16_t ADCBuf_convert ( ADCBuf_Handle  handle,
ADCBuf_Conversion  conversions[],
uint_fast8_t  channelCount 
)

This function starts a set of conversions on one or more channels.

Parameters
handleAn ADCBuf handle returned from ADCBuf_open()
conversionsA pointer to an array of ADCBuf_Conversion structs with the specific parameters for each channel. Only use one ADCBuf_Conversion struct per channel.
channelCountThe number of channels to convert on in this call. Should be the length of the conversions array. Depending on the device, multiple simultaneous conversions may not be supported. See device specific implementation.
Returns
ADCBuf_STATUS_SUCCESS if the operation was successful. ADCBuf_STATUS_ERROR or a device specific status is returned otherwise.
Precondition
ADCBuf_open() must have been called prior.
See also
ADCBuf_convertCancel()
int_fast16_t ADCBuf_convertCancel ( ADCBuf_Handle  handle)

This function cancels an ADC conversion that is in progress.

This function must be called before calling ADCBuf_close().

Parameters
handleAn ADCBuf handle returned from ADCBuf_open()
Returns
ADCBuf_STATUS_SUCCESS if the operation was successful. ADCBuf_STATUS_ERROR or a device specific status is returned otherwise.
See also
ADCBuf_convert()
uint_fast8_t ADCBuf_getResolution ( ADCBuf_Handle  handle)

This function returns the resolution in bits of the specified ADC.

Parameters
handleAn ADCBuf handle returned from ADCBuf_open().
Returns
The resolution in bits of the specified ADC.
Precondition
ADCBuf_open() must have been called prior.
int_fast16_t ADCBuf_adjustRawValues ( ADCBuf_Handle  handle,
void *  sampleBuffer,
uint_fast16_t  sampleCount,
uint32_t  adcChannel 
)

This function adjusts a raw ADC output buffer such that the result is comparable between devices of the same make. The function does the adjustment in-place.

Parameters
handleAn ADCBuf handle returned from ADCBuf_open().
sampleBufferA buffer full of raw sample values.
sampleCountThe number of samples to adjust.
adcChannelThe channel the buffer was sampled on.
Returns
A buffer full of adjusted samples contained in sampleBuffer.
ADCBuf_STATUS_SUCCESS if the operation was successful. ADCBuf_STATUS_ERROR or a device specific status is returned otherwise.
Precondition
ADCBuf_open() must have been called prior.
int_fast16_t ADCBuf_convertAdjustedToMicroVolts ( ADCBuf_Handle  handle,
uint32_t  adcChannel,
void *  adjustedSampleBuffer,
uint32_t  outputMicroVoltBuffer[],
uint_fast16_t  sampleCount 
)

This function converts a raw ADC output value to a value scaled in micro volts.

Parameters
handleAn ADCBuf handle returned from ADCBuf_open()
adcChannelThe ADC channel the samples stem from. This parameter is only necessary for certain devices. See device specific implementation for details.
adjustedSampleBufferA buffer full of adjusted samples.
outputMicroVoltBufferThe output buffer. The conversion does not occur in place due to the differing data type sizes.
sampleCountThe number of samples to convert.
Returns
A number of measurements scaled in micro volts inside outputMicroVoltBuffer.
ADCBuf_STATUS_SUCCESS if the operation was successful. ADCBuf_STATUS_ERROR or a device specific status is returned otherwise.
Precondition
ADCBuf_open() must have been called prior.
ADCBuf_adjustRawValues() must be called on adjustedSampleBuffer prior.
Copyright 2016, Texas Instruments Incorporated