|
ESMO_Handle | ESMO_init (void *pMemory, const size_t numBytes) |
| Initializes the ESMO controller. More...
|
|
void | ESMO_resetParams (ESMO_Handle handle) |
| Reset the ESMO controller. More...
|
|
void | ESMO_setParams (ESMO_Handle handle, const USER_Params *pUserParams) |
| Set the ESMO controller. More...
|
|
void | ESMO_setPLLParams (ESMO_Handle handle, const float32_t pll_KpMax, const float32_t pll_KpMin, const float32_t pll_KpSF) |
| Set PLL parameters for the ESMO controller. More...
|
|
void | ESMO_setPLLKi (ESMO_Handle handle, const float32_t pll_Ki) |
| Set PLL parameters for the ESMO controller. More...
|
|
static void | ESMO_setBEMFThreshold (ESMO_Handle handle, const float32_t bemfThreshold) |
| Set kp of the pll for the ESMO controller. More...
|
|
static void | ESMO_setPLLKpSF (ESMO_Handle handle, const float32_t pll_KpSF) |
| Set kp of the pll for the ESMO controller. More...
|
|
void | ESMO_setKslideParams (ESMO_Handle handle, const float32_t KslideMax, const float32_t KslideMin) |
| Set PLL parameters for the ESMO controller. More...
|
|
static void | ESMO_setKslide (ESMO_Handle handle, const float32_t Kslide) |
| Sets Kslide for the ESMO controller. More...
|
|
void | ESMO_updateFilterParams (ESMO_Handle handle) |
| Reset the ESMO controller. More...
|
|
void | ESMO_updatePLLParams (ESMO_Handle handle) |
| Reset the ESMO controller. More...
|
|
void | ESMO_full_run (ESMO_Handle handle, float32_t Vdcbus, MATH_vec3 *pVabc_pu, MATH_vec2 *pIabVec) |
| Runs the ESMO controller. More...
|
|
static void | ESMO_resetPLL (ESMO_Handle handle) |
| Resets PLL integration for the ESMO controller. More...
|
|
static void | ESMO_setOffsetCoef (ESMO_Handle handle, const float32_t offsetSF) |
| Sets angle offset coefficient for the ESMO controller. More...
|
|
static void | ESMO_setBEMFKslfFreq (ESMO_Handle handle, const float32_t filterFc_Hz) |
| Sets speed filter cut off frequency for the ESMO controller. More...
|
|
static void | ESMO_setSpeedFilterFreq (ESMO_Handle handle, const float32_t lpfFc_Hz) |
| Sets speed filter cut off frequency for the ESMO controller. More...
|
|
static void | ESMO_setPLLKp (ESMO_Handle handle, const float32_t pll_Kp) |
| Runs the ESMO controller. More...
|
|
static void | ESMO_setAnglePu (ESMO_Handle handle, const float32_t theta_rad) |
| Set Angle to the ESMO controller. More...
|
|
static void | ESMO_setPLLSpeedPu (ESMO_Handle handle, const float32_t speed_Hz) |
| Set Angle to the ESMO controller. More...
|
|
static void | ESMO_setSpeedRef (ESMO_Handle handle, const float32_t speedRef_Hz) |
| Set reference speed to the ESMO controller. More...
|
|
static float32_t | ESMO_getSpeed_Hz (ESMO_Handle handle) |
| Gets the speed from the ESMO controller. More...
|
|
static float32_t | ESMO_getSpeedPLL_Hz (ESMO_Handle handle) |
| Gets the PLL speed from the ESMO controller. More...
|
|
static float32_t | ESMO_getAnglePLL (ESMO_Handle handle) |
| Gets the PLL angle from the ESMO controller. More...
|
|
static float32_t | ESMO_getAngleElec (ESMO_Handle handle) |
| Gets the angle from the ESMO controller. More...
|
|
static void | ESMO_updateKslide (ESMO_Handle handle) |
| Update Kslide for the ESMO controller. More...
|
|
static void | ESMO_run (ESMO_Handle handle, float32_t Vdcbus, MATH_vec3 *pVabc_pu, MATH_vec2 *pIabVec) |
|