Go to the source code of this file.
Data Structures | |
struct | _HALL_Obj_ |
Defines the HALL controller object. More... | |
Macros | |
#define | HALL_calcAngle HALL_run |
Runs the HALL controller. More... | |
Typedefs | |
typedef struct _HALL_Obj_ | HALL_Obj |
Defines the HALL controller object. More... | |
typedef struct _HALL_Obj_ * | HALL_Handle |
Defines the HALL handle. More... | |
Enumerations | |
enum | HALL_Status_e { HALL_IDLE = 0, HALL_ALIGNMENT = 1, HALL_CALIBRATION = 2, HALL_RUN = 3 } |
Functions | |
HALL_Handle | HALL_init (void *pMemory, const size_t numBytes) |
Initializes the HALL controller. More... | |
void | HALL_setParams (HALL_Handle handle, const USER_Params *pUserParams) |
Sets the hall estimator parameters. More... | |
void | HALL_setAngleBuf (HALL_Handle handle, const float32_t *ptrAngleBuf) |
Sets the angle buffer value for hall estimator. More... | |
void | HALL_resetParams (HALL_Handle handle) |
Resets the hall estimator parameters. More... | |
void | HALL_setGPIOs (HALL_Handle handle, const uint16_t gpioHallU, const uint16_t gpioHallV, const uint16_t gpioHallW) |
Sets GPIO for hall sensors input. More... | |
static float32_t | HALL_getSpeed_Hz (HALL_Handle handle) |
Gets the feedback speed from hall estimator. More... | |
static void | HALL_setSpeed_Hz (HALL_Handle handle, const float32_t speedHall_Hz) |
Sets a value to the speed for the hall estimator. More... | |
static void | HALL_setTimeStamp (HALL_Handle handle, const uint32_t timeStamp) |
Sets a value to the time stamp for the hall estimator. More... | |
static float32_t | HALL_getAngle_rad (HALL_Handle handle) |
Gets the angle from the hall estimator, rad. More... | |
static uint16_t | HALL_getInputState (HALL_Handle handle) |
Gets the hall sensors input GPIO state. More... | |
static void | HALL_setForceAngleAndIndex (HALL_Handle handle, float32_t speedRef) |
Sets the force angle and index for next step of the hall estimator. More... | |
static void | HALL_run (HALL_Handle handle, float32_t speedRef) |