![]() |
![]() |
| ADC.h | Analog to Digital Conversion (ADC) Input Driver |
| ADCBuf.h | Analog to Digital Conversion Buffer (ADCBuf) Input Driver |
| ADCBufLPF3.h | ADCBuf driver implementation for an LPF3 analog-to-digital converter |
| ADCLPF3.h | ADC driver implementation for the ADC peripheral on Low Power F3 devices |
| AnsiColor.h | |
| APULPF3.h | PRELIMINARY APU driver interface |
| APULPF3_FW.h | |
| BatMonSupportLPF3.h | BatMon Support layer |
| BatteryMonitor.h | Battery Monitor driver |
| BatteryMonitorLPF3.h | Battery Monitor driver implementation for the LPF3 family |
| Board.h | Portable board-specific symbols |
| Button.h | Button driver |
| CAN.h | Controller Area Network (CAN) Driver Interface |
| CANCC27XX.h | CAN driver implementation for the CC27XX family |
| CANMCAN.h | Common CAN functions for MCAN configuration |
| ClockP.h | Clock interface for the RTOS Porting Interface |
| ClockPLPF3.h | |
| Comparator.h | Comparator Driver |
| ComparatorLPF3LP.h | |
| DebugP.h | Debug support |
| Display.h | Generic interface for text output |
| DisplayHost.h | Display driver for printf-like output |
| DisplayUart2.h | Display.h implementation for UART output |
| Driver_Init.h | |
| EventP.h | Event Group support |
| GPIO.h | General Purpose I/O driver interface |
| GPIOLPF3.h | GPIO driver implementation for Low Power F3 devices |
| hw_cpu_dwt.h | |
| hw_cpu_itm.h | |
| hw_cpu_scs.h | |
| hw_cpu_tpiu.h | |
| HwiP.h | Hardware Interrupt module for the RTOS Porting Interface |
| I2C.h | Inter-Integrated Circuit (I2C) Controller Driver |
| I2CLPF3.h | I2C driver implementation for a Low Power F3 device I2C controller |
| I2CSupport.h | Holder of common helper functions for the I2C driver |
| I2CTarget.h | I2CTarget driver interface |
| I2CTargetLPF3.h | I2CTarget driver implementation for a Low Power F3 device I2C target |
| I2S.h | Inter-Integrated Circuit Sound (I2S) Bus Driver |
| I2SLPF3.h | I2S driver implementation for LPF3 devices |
| ITM.h | ITM driver header |
| ITMLPF3.h | CC27XX specific ITM implementation |
| LED.h | LED driver |
| LGPTimerLPF3.h | LGPTimer driver implementation for Low Power F3 devices |
| List.h | Linked List interface for use in drivers |
| LogSinkBuf.h | |
| LogSinkITM.h | PRELIMINARY LogSinkITM interface |
| LogSinkTraceLPF3.h | PRELIMINARY LogSinkTraceLPF3 interface |
| LogSinkUART.h | PRELIMINARY LogSinkUART interface |
| Math.h | Math utility functions |
| MCAN.h | Hardware abstraction layer for M_CAN Controller v3.2.1 |
| MCAN_reg.h | M_CAN controller v3.2.1 register definitions |
| MessageQueueP.h | MessageQueue module for the RTOS Porting Interface |
| MutexP.h | Mutex module for the RTOS Porting Interface |
| NoRTOS.h | NoRTOS framework module |
| NVS.h | Non-Volatile Storage driver interface |
| NVSLPF3.h | Non-Volatile Storage driver for Low Power F3 devices |
| NVSRAM.h | RAM implementation of the NVS driver |
| NVSSPI25X.h | Non-Volatile Storage driver implementation for SPI flash peripherals |
| Power.h | Power Manager |
| PowerCC23X0.h | Power manager interface for CC23X0 devices |
| PowerCC27XX.h | Power manager interface for CC27XX |
| PowerCC27XX_s.h | Interface for Secure Power driver for CC27XX. Not to be used by non-secure application |
| PowerCC27XX_veneers.h | Secure Power API functions available from non-secure context through veneers |
| PWM.h | Pulse Width Modulation (PWM) driver |
| PWMTimerLPF3.h | PWM driver implementation for Low Power F3 devices |
| QueueP.h | |
| RingBuf.h | |
| SD.h | Secure Digital (SD) Driver |
| SDFatFS.h | File Allocation Table File System (FATFS) Driver |
| SDSPI.h | SD driver implementation built on the TI SPI driver |
| SecureCallback.h | |
| SecureCallback_s.h | |
| SemaphoreP.h | Semaphore module for the RTOS Porting Interface |
| SPI.h | Serial Peripheral Interface (SPI) Driver Interface |
| spiffs.h | |
| SPIFFSNVS.h | Module to enable the SPI Flash File System (SPIFFS) on the TI NVS driver |
| SPILPF3DMA.h | SPI driver implementation for a Low Power F3 device SPI controller using the UDMA controller |
| StructRingBuf.h | |
| SwiP.h | Software Interrupt module for the RTOS Porting Interface |
| SystemP.h | System module for the RTOS Porting Interface |
| TaskP.h | Task module for the RTOS Porting Interface |
| TCAN455X.h | TCAN455X Driver Interface |
| TCAN455X_reg.h | TCAN455X device-specific register definitions |
| Temperature.h | Temperature driver |
| TemperatureLPF3.h | Temperature driver implementation for the Low Power F3 family |
| TimestampP.h | Timestamp module for the RTOS Porting Interface |
| types.h | |
| UART2.h | PRELIMINARY UART driver interface |
| UART2LPF3.h | UART driver implementation for a Low Power F3 device UART controller |
| UART2Support.h | Holder of common helper functions for the UART driver |
| UDMALPF3.h | UDMALPF3 driver implementation |
| unistd.h | |
| Watchdog.h | Watchdog driver interface |
| WatchdogLPF3.h | Watchdog driver implementation for Low Power F3 devices |