Contains public interface to various functions related to the DRV8353 object.
|
enum | DRV8353_CtrlMode_e {
DRV8353_CTRLMODE_WRITE = 0,
DRV8353_CTRLMODE_READ = 1
} |
| Enumeration for the R/W modes. More...
|
|
enum | DRV8353_Address_e {
DRV8353_ADDRESS_STATUS_0 = (0 << 11),
DRV8353_ADDRESS_STATUS_1 = (1 << 11),
DRV8353_ADDRESS_CONTROL_2 = (2 << 11),
DRV8353_ADDRESS_CONTROL_3 = (3 << 11),
DRV8353_ADDRESS_CONTROL_4 = (4 << 11),
DRV8353_ADDRESS_CONTROL_5 = (5 << 11),
DRV8353_ADDRESS_CONTROL_6 = (6 << 11),
DRV8353_ADDRESS_CONTROL_7 = (7 << 11)
} |
| Enumeration for the register addresses. More...
|
|
enum | DRV8353_STATUS00_WarningWatchdog_e {
DRV8353_VDS_LC = (1 << 0),
DRV8353_VDS_HC = (1 << 1),
DRV8353_VDS_LB = (1 << 2),
DRV8353_VDS_HB = (1 << 3),
DRV8353_VDS_LA = (1 << 4),
DRV8353_VDS_HA = (1 << 5),
DRV8353_OTSD = (1 << 6),
DRV8353_UVLO = (1 << 7),
DRV8353_GDF = (1 << 8),
DRV8353_VDS_OCP = (1 << 9),
DRV8353_FAULT = (1 << 10)
} |
| Enumeration for the Status 0 register, faults. More...
|
|
enum | DRV8353_STATUS01_OvVdsFaults_e {
DRV8353_VGS_LC = (1 << 0),
DRV8353_VGS_HC = (1 << 1),
DRV8353_VGS_LB = (1 << 2),
DRV8353_VGS_HB = (1 << 3),
DRV8353_VGS_LA = (1 << 4),
DRV8353_VGS_HA = (1 << 5),
DRV8353_CPUV = (1 << 6),
DRV8353_OTW = (1 << 7),
DRV8353_SC_OC = (1 << 8),
DRV8353_SB_OC = (1 << 9),
DRV8353_SA_OC = (1 << 10)
} |
| Enumeration for the Status 1 register, OV/VDS faults. More...
|
|
enum | DRV8353_CTRL02_PWMMode_e {
DRV8353_PWMMODE_6 = 0,
DRV8353_PWMMODE_3 = 1,
DRV8353_PWMMODE_1 = 2
} |
| Enumeration for the driver PWM mode. More...
|
|
enum | DRV8353_CTRL03_PeakSourCurHS_e {
DRV8353_ISOUR_HS_0P010_A = 0,
DRV8353_ISOUR_HS_0P030_A = 1,
DRV8353_ISOUR_HS_0P060_A = 2,
DRV8353_ISOUR_HS_0P080_A = 3,
DRV8353_ISOUR_HS_0P120_A = 4,
DRV8353_ISOUR_HS_0P140_A = 5,
DRV8353_ISOUR_HS_0P170_A = 6,
DRV8353_ISOUR_HS_0P190_A = 7,
DRV8353_ISOUR_HS_0P260_A = 8,
DRV8353_ISOUR_HS_0P330_A = 9,
DRV8353_ISOUR_HS_0P370_A = 10,
DRV8353_ISOUR_HS_0P440_A = 11,
DRV8353_ISOUR_HS_0P570_A = 12,
DRV8353_ISOUR_HS_0P680_A = 13,
DRV8353_ISOUR_HS_0P820_A = 14,
DRV8353_ISOUR_HS_1P000_A = 15
} |
| Enumeration for the high side gate drive peak source current; gate currents not consistent with DS. More...
|
|
enum | DRV8353_CTRL03_PeakSinkCurHS_e {
DRV8353_ISINK_HS_0P020_A = 0,
DRV8353_ISINK_HS_0P060_A = 1,
DRV8353_ISINK_HS_0P120_A = 2,
DRV8353_ISINK_HS_0P160_A = 3,
DRV8353_ISINK_HS_0P240_A = 4,
DRV8353_ISINK_HS_0P280_A = 5,
DRV8353_ISINK_HS_0P340_A = 6,
DRV8353_ISINK_HS_0P380_A = 7,
DRV8353_ISINK_HS_0P520_A = 8,
DRV8353_ISINK_HS_0P660_A = 9,
DRV8353_ISINK_HS_0P740_A = 10,
DRV8353_ISINK_HS_0P880_A = 11,
DRV8353_ISINK_HS_1P140_A = 12,
DRV8353_ISINK_HS_1P360_A = 13,
DRV8353_ISINK_HS_1P640_A = 14,
DRV8353_ISINK_HS_2P000_A = 15
} |
| Enumeration for the high side gate drive peak sink current; gate currents not consistent with DS. More...
|
|
enum | DRV8353_CTRL03_Lock_e {
DRV8353_LOCK_UNLOCK = 3,
DRV8353_LOCK_LOCK = 6
} |
| Enumeration for the high side and low side gate drive peak source time; adapt timings to DRV8353. More...
|
|
enum | DRV8353_CTRL04_PeakTime_e {
DRV8353_TSOUR_500_NS = 0,
DRV8353_TSOUR_1000_NS = 1,
DRV8353_TSOUR_2000_NS = 2,
DRV8353_TSOUR_4000_NS = 3
} |
| Enumeration for the high side and low side gate drive peak source time; adapt timings to DRV8353. More...
|
|
enum | DRV8353_CTRL04_PeakSourCurLS_e {
DRV8353_ISOUR_LS_0P010_A = 0,
DRV8353_ISOUR_LS_0P030_A = 1,
DRV8353_ISOUR_LS_0P060_A = 2,
DRV8353_ISOUR_LS_0P080_A = 3,
DRV8353_ISOUR_LS_0P120_A = 4,
DRV8353_ISOUR_LS_0P140_A = 5,
DRV8353_ISOUR_LS_0P170_A = 6,
DRV8353_ISOUR_LS_0P190_A = 7,
DRV8353_ISOUR_LS_0P260_A = 8,
DRV8353_ISOUR_LS_0P330_A = 9,
DRV8353_ISOUR_LS_0P370_A = 10,
DRV8353_ISOUR_LS_0P440_A = 11,
DRV8353_ISOUR_LS_0P570_A = 12,
DRV8353_ISOUR_LS_0P680_A = 13,
DRV8353_ISOUR_LS_0P820_A = 14,
DRV8353_ISOUR_LS_1P000_A = 15
} |
| Enumeration for the low side gate drive peak source current; adapt current ratings. More...
|
|
enum | DRV8353_CTRL04_PeakSinkCurLS_e {
DRV8353_ISINK_LS_0P020_A = 0,
DRV8353_ISINK_LS_0P060_A = 1,
DRV8353_ISINK_LS_0P120_A = 2,
DRV8353_ISINK_LS_0P160_A = 3,
DRV8353_ISINK_LS_0P240_A = 4,
DRV8353_ISINK_LS_0P280_A = 5,
DRV8353_ISINK_LS_0P340_A = 6,
DRV8353_ISINK_LS_0P380_A = 7,
DRV8353_ISINK_LS_0P520_A = 8,
DRV8353_ISINK_LS_0P660_A = 9,
DRV8353_ISINK_LS_0P740_A = 10,
DRV8353_ISINK_LS_0P880_A = 11,
DRV8353_ISINK_LS_1P140_A = 12,
DRV8353_ISINK_LS_1P360_A = 13,
DRV8353_ISINK_LS_1P640_A = 14,
DRV8353_ISINK_LS_2P000_A = 15
} |
| Enumeration for the low side gate drive peak sink current; adapt current ratings. More...
|
|
enum | DRV8353_CTRL05_VDSLVL_e {
DRV8353_VDS_LEVEL_0P060_V = 0,
DRV8353_VDS_LEVEL_0P130_V = 1,
DRV8353_VDS_LEVEL_0P200_V = 2,
DRV8353_VDS_LEVEL_0P260_V = 3,
DRV8353_VDS_LEVEL_0P310_V = 4,
DRV8353_VDS_LEVEL_0P450_V = 5,
DRV8353_VDS_LEVEL_0P530_V = 6,
DRV8353_VDS_LEVEL_0P600_V = 7,
DRV8353_VDS_LEVEL_0P680_V = 8,
DRV8353_VDS_LEVEL_0P750_V = 9,
DRV8353_VDS_LEVEL_0P940_V = 10,
DRV8353_VDS_LEVEL_1P130_V = 11,
DRV8353_VDS_LEVEL_1P300_V = 12,
DRV8353_VDS_LEVEL_1P500_V = 13,
DRV8353_VDS_LEVEL_1P700_V = 14,
DRV8353_VDS_LEVEL_1P880_V = 15
} |
| Enumeration for the VDS comparator threshold. More...
|
|
enum | DRV8353_CTRL05_OcpDeg_e {
DRV8353_VDSDEG_2_US = 0,
DRV8353_VDSDEG_4_US = 1,
DRV8353_VDSDEG_6_US = 2,
DRV8353_VDSDEG_8_US = 3
} |
| Enumeration for the OCP/VDS sense deglitch time; adapt deglitch time comments. More...
|
|
enum | DRV8353_CTRL05_OcpMode_e {
DRV8353_LATCHED_SHUTDOWN = 0,
DRV8353_AUTOMATIC_RETRY = 1,
DRV8353_REPORT_ONLY = 2,
DRV8353_DISABLE_OCP = 3
} |
| Enumeration for the OCP report mode. More...
|
|
enum | DRV8353_CTRL05_DeadTime_e {
DRV8353_DEADTIME_50_NS = 0,
DRV8353_DEADTIME_100_NS = 1,
DRV8353_DEADTIME_200_NS = 2,
DRV8353_DEADTIME_400_NS = 3
} |
| Enumeration for the driver dead time. More...
|
|
enum | DRV8353_CTRL06_SENLevel_e {
DRV8353_SEN_Lvl_Ocp_0p25 = 0,
DRV8353_SEN_Lvl_Ocp_0p50 = 1,
DRV8353_SEN_Lvl_Ocp_0p75 = 2,
DRV8353_SEN_Lvl_Ocp_1p00 = 3
} |
| Enumeration for the Sense OCP level. More...
|
|
enum | DRV8353_CTRL06_CSAGain_e {
DRV8353_Gain_5VpV = 0,
DRV8353_Gain_10VpV = 1,
DRV8353_Gain_20VpV = 2,
DRV8353_Gain_40VpV = 3
} |
| Enumeration for the gain of shunt amplifier. More...
|
|
|
DRV8353_Handle | DRV8353_init (void *pMemory) |
| Initializes the DRV8353 object. More...
|
|
static DRV_Word_t | DRV8353_buildCtrlWord (const DRV8353_CtrlMode_e ctrlMode, const DRV8353_Address_e regAddr, const uint16_t data) |
| Builds the control word. More...
|
|
void | DRV8353_enable (DRV8353_Handle handle) |
| Enables the DRV8353. More...
|
|
void | DRV8353_setSPIHandle (DRV8353_Handle handle, uint32_t spiHandle) |
| Sets the SPI handle in the DRV8353. More...
|
|
void | DRV8353_setGPIOCSNumber (DRV8353_Handle handle, uint32_t gpioNumber) |
| Sets the GPIO number in the DRV8353. More...
|
|
void | DRV8353_setGPIOENNumber (DRV8353_Handle handle, uint32_t gpioNumber) |
| Sets the GPIO number in the DRV8353. More...
|
|
static void | DRV8353_resetEnableTimeout (DRV8353_Handle handle) |
| Resets the enable timeout flag. More...
|
|
static void | DRV8353_resetRxTimeout (DRV8353_Handle handle) |
| Resets the RX fifo timeout flag. More...
|
|
void | DRV8353_setupSPI (DRV8353_Handle handle, DRV8353_VARS_t *drv8353Vars) |
| Initialize the interface to all 8320 SPI variables. More...
|
|
uint16_t | DRV8353_readSPI (DRV8353_Handle handle, const DRV8353_Address_e regAddr) |
| Reads data from the DRV8353 register. More...
|
|
void | DRV8353_writeSPI (DRV8353_Handle handle, const DRV8353_Address_e regAddr, const uint16_t data) |
| Writes data to the DRV8353 register. More...
|
|
void | DRV8353_writeData (DRV8353_Handle handle, DRV8353_VARS_t *drv8353Vars) |
| Write to the DRV8353 SPI registers. More...
|
|
void | DRV8353_readData (DRV8353_Handle handle, DRV8353_VARS_t *drv8353Vars) |
| Read from the DRV8353 SPI registers. More...
|
|